Modules#
Messaging Client#
API and Callbacks for the Messaging Cluster Client Component.
Silicon Labs implementation of the Messaging client cluster. This component requires extending to display the message on the hardware display.
API#
Clear the message.
Print information about the message.
Confirm a message.
API Documentation#
emAfPluginMessagingClientClearMessage#
void emAfPluginMessagingClientClearMessage (uint8_t endpoint)
Clear the message.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | N/A | endpoint | The relevant endpoint. |
This function is used to manually inactivate or clear the message.
emAfPluginMessagingClientPrintInfo#
void emAfPluginMessagingClientPrintInfo (uint8_t endpoint)
Print information about the message.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | N/A | endpoint | The relevant endpoint. |
emberAfPluginMessagingClientConfirmMessage#
EmberAfStatus emberAfPluginMessagingClientConfirmMessage (uint8_t endpoint)
Confirm a message.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | N/A | endpoint |
This function is used to confirm a message. The messaging client plugin sends the confirmation command to the endpoint on the node that sent the message.
Returns
EMBER_ZCL_STATUS_SUCCESS if the confirmation was sent, EMBER_ZCL_STATUS_FAILURE if an error occurred, or EMBER_ZCL_STATUS_NOT_FOUND if the message does not exist.