Modules#

Level Control

Level Control Server#

API and Callbacks for the Level Control Cluster Server Component.

Silicon Labs implementation of the Level Control server cluster. If the ZLL Level Control server cluster component is also enabled, this component uses it to handle ZLL enhancements. Otherwise, all ZLL extensions are disabled. It is not intended for production but provides sample code to show how the cluster could be implemented.

This group describes the CLI commands for the Level Control cluster. Listed below is a description of the cluster: Attributes and commands for controlling devices that can be set to a level between fully 'On' and fully 'Off.'

Macros#

#define
EMBER_AF_PLUGIN_LEVEL_CONTROL_TICK_TIME (MILLISECOND_TICKS_PER_SECOND / EMBER_AF_PLUGIN_LEVEL_CONTROL_TICKS_PER_SECOND)
#define

zcl level-control mv-to-level [level:1] [transitionTime:2] [optionMask:1] [optionOverride:1]

#define

zcl level-control move [moveMode:1] [rate:1] [optionMask:1] [optionOverride:1]

#define

zcl level-control step [stepMode:1] [stepSize:1] [transitionTime:2] [optionMask:1] [optionOverride:1]

#define

zcl level-control stop [optionMask:1] [optionOverride:1]

#define

zcl level-control o-mv-to-level [level:1] [transitionTime:2]

#define

zcl level-control o-move [moveMode:1] [rate:1]

#define

zcl level-control o-step [stepMode:1] [stepSize:1] [transitionTime:2]

#define
#define

zcl level-control mv-to-closest-freq [frequency:2]

Macro Definition Documentation#

EMBER_AF_PLUGIN_LEVEL_CONTROL_TICKS_PER_SECOND#

#define EMBER_AF_PLUGIN_LEVEL_CONTROL_TICKS_PER_SECOND
Value:
32

EMBER_AF_PLUGIN_LEVEL_CONTROL_TICK_TIME#

#define EMBER_AF_PLUGIN_LEVEL_CONTROL_TICK_TIME
Value:
  (MILLISECOND_TICKS_PER_SECOND / EMBER_AF_PLUGIN_LEVEL_CONTROL_TICKS_PER_SECOND)

EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_LEVEL#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_LEVEL

zcl level-control mv-to-level [level:1] [transitionTime:2] [optionMask:1] [optionOverride:1]

  • Command description for MoveToLevel

    • level - INT8U

    • transitionTime - INT16U

    • optionMask - BITMAP8

    • optionOverride - BITMAP8


EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MOVE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MOVE

zcl level-control move [moveMode:1] [rate:1] [optionMask:1] [optionOverride:1]

  • Command description for Move

    • moveMode - MoveMode [ENUM8]

    • rate - INT8U

    • optionMask - BITMAP8

    • optionOverride - BITMAP8 See Also


EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STEP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STEP

zcl level-control step [stepMode:1] [stepSize:1] [transitionTime:2] [optionMask:1] [optionOverride:1]

  • Command description for Step

    • stepMode - StepMode [ENUM8]

    • stepSize - INT8U

    • transitionTime - INT16U

    • optionMask - BITMAP8

    • optionOverride - BITMAP8 See Also


EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STOP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STOP

zcl level-control stop [optionMask:1] [optionOverride:1]

  • Command description for Stop

    • optionMask - BITMAP8

    • optionOverride - BITMAP8


EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MV_TO_LEVEL#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MV_TO_LEVEL

zcl level-control o-mv-to-level [level:1] [transitionTime:2]

  • Command description for MoveToLevelWithOnOff

    • level - INT8U

    • transitionTime - INT16U


EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MOVE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MOVE

zcl level-control o-move [moveMode:1] [rate:1]

  • Command description for MoveWithOnOff


EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STEP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STEP

zcl level-control o-step [stepMode:1] [stepSize:1] [transitionTime:2]

  • Command description for StepWithOnOff

    • stepMode - StepMode [ENUM8]

    • stepSize - INT8U

    • transitionTime - INT16U See Also


EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STOP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STOP

zcl level-control o-stop

  • Command description for StopWithOnOff


EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_CLOSEST_FREQ#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_CLOSEST_FREQ

zcl level-control mv-to-closest-freq [frequency:2]

  • Command description for MoveToClosestFrequency

    • frequency - INT16U