You are viewing documentation for version:
DMP UI Demo Stub#
API and Callbacks for the DMP UI Demo Stub Component.
This component provides stubs for the DynamicMultiprotocolDemoLight app. Use this component to satisfy compilation when the display driver is not used, primarily when the Dynamic Multiprotocol UI Demo Code component is not enabled.
API#
enum
DMP_UI_LIGHT_ON
DMP_UI_LIGHT_OFF
DMP_UI_LIGHT_UNCHANGED
DMP_UI_LIGHT_OFF
DMP_UI_LIGHT_ON
DMP_UI_LIGHT_UNCHANGED
}
API Documentation#
sl_dmp_ui_light_state_t#
sl_dmp_ui_light_state_t
| Enumerator |
|---|
| DMP_UI_LIGHT_ON | |
| DMP_UI_LIGHT_OFF | |
| DMP_UI_LIGHT_UNCHANGED | |
| DMP_UI_LIGHT_OFF | |
| DMP_UI_LIGHT_ON | |
| DMP_UI_LIGHT_UNCHANGED | |
sl_dmp_ui_display_zigbee_state#
#define sl_dmp_ui_display_zigbee_state
sl_dmp_ui_zigbee_permit_join#
#define sl_dmp_ui_zigbee_permit_join
sl_dmp_ui_light_off#
#define sl_dmp_ui_light_off
sl_dmp_ui_light_on#
#define sl_dmp_ui_light_on
sl_dmp_ui_update_direction#
#define sl_dmp_ui_update_direction
sl_dmp_ui_bluetooth_connected#
#define sl_dmp_ui_bluetooth_connected
sl_dmp_ui_set_ble_device_name#
#define sl_dmp_ui_set_ble_device_name
sl_dmp_ui_init#
#define sl_dmp_ui_init
sl_dmp_ui_display_help#
#define sl_dmp_ui_display_help
DMP_UI_DIRECTION_INVALID#
#define DMP_UI_DIRECTION_INVALID
Value:0
DMP_UI_DIRECTION_BLUETOOTH#
#define DMP_UI_DIRECTION_BLUETOOTH
Value:1
DMP_UI_DIRECTION_SWITCH#
#define DMP_UI_DIRECTION_SWITCH
Value:2
DMP_UI_DIRECTION_ZIGBEE#
#define DMP_UI_DIRECTION_ZIGBEE
Value:3
DmpUiLightDirection_t#
#define DmpUiLightDirection_t
Value:uint8_t
sl_dmp_ui_set_light_direction#
#define sl_dmp_ui_set_light_direction
sl_dmp_ui_get_light_direction#
#define sl_dmp_ui_get_light_direction
Value:(...)