Metering Server#
API and Callbacks for the Metering Cluster Server Component.
This is an implementation of the simple metering server. It supports the required current summation delivered attribute (0x0000), power factor(0x0006), status(0x0200), hours in operation (0x0202), unit of measure (0x0300, multiplier (0x0301), divisor(0x0302), summation formatting (0x0303), metering device type (0x0306), current partial profile interval start time delivered (0x0405), and current partial profile interval value delivered(0x0407).
API#
void
emberAfPluginMeteringServerEnableFastPolling(bool enableFastPolling)
Set the fast polling mode.
API Documentation#
emberAfPluginMeteringServerEnableFastPolling#
void emberAfPluginMeteringServerEnableFastPolling (bool enableFastPolling)
Set the fast polling mode.
Parameters
Type | Direction | Argument Name | Description |
---|---|---|---|
bool | N/A | enableFastPolling | False: disable, True: enable. |
Enables and disables fast polling mode.