Messaging Client#

Callbacks for Messaging Client Component.

Callbacks#

bool
emberAfPluginMessagingClientPreDisplayMessageCallback(uint32_t messageId, uint8_t messageControl, uint32_t startTime, uint16_t durationInMinutes, uint8_t *message, uint8_t optionalExtendedMessageControl)

Pre Display Message.

void
emberAfPluginMessagingClientDisplayMessageCallback(EmberAfPluginMessagingClientMessage *message)

Display a message.

void
emberAfPluginMessagingClientCancelMessageCallback(EmberAfPluginMessagingClientMessage *message)

Cancel a message.

Callbacks Documentation#

emberAfPluginMessagingClientPreDisplayMessageCallback#

bool emberAfPluginMessagingClientPreDisplayMessageCallback (uint32_t messageId, uint8_t messageControl, uint32_t startTime, uint16_t durationInMinutes, uint8_t * message, uint8_t optionalExtendedMessageControl)

Pre Display Message.

Parameters
TypeDirectionArgument NameDescription
uint32_tN/AmessageId

Ver.: always

uint8_tN/AmessageControl

Ver.: always

uint32_tN/AstartTime

Ver.: always

uint16_tN/AdurationInMinutes

Ver.: always

uint8_t *N/Amessage

Ver.: always

uint8_tN/AoptionalExtendedMessageControl

Ver.: always

This function is called by the Messaging client plugin when a DisplayMessage command is received. If callback returns true, the plugin assumes the message have been handled and will not do anything with the message. Otherwise, the plugin will go through with its own implementation.


emberAfPluginMessagingClientDisplayMessageCallback#

void emberAfPluginMessagingClientDisplayMessageCallback (EmberAfPluginMessagingClientMessage * message)

Display a message.

Parameters
TypeDirectionArgument NameDescription
EmberAfPluginMessagingClientMessage *N/Amessage

The message that should be displayed. Ver.: always

This function is called by the messaging client plugin whenever the application should display a message.


emberAfPluginMessagingClientCancelMessageCallback#

void emberAfPluginMessagingClientCancelMessageCallback (EmberAfPluginMessagingClientMessage * message)

Cancel a message.

Parameters
TypeDirectionArgument NameDescription
EmberAfPluginMessagingClientMessage *N/Amessage

The message that should no longer be displayed. Ver.: always

This function is called by the messaging client plugin whenever the application should stop displaying a message.