Cluster Commands: Door Lock#
This group describes the CLI commands for the Door Lock cluster. Listed below is a description of the cluster: Provides an interface into a generic way to secure a door.
Macros#
zcl lock lock [PIN:-1]
zcl lock unlock [PIN:-1]
zcl lock toggle [pin:-1]
zcl lock unlock-with-timeout [timeoutInSeconds:2] [pin:-1]
zcl lock get-log-record [logIndex:2]
zcl lock set-pin [userId:2] [userStatus:1] [userType:1] [pin:-1]
zcl lock get-pin [userId:2]
zcl lock clear-pin [userId:2]
zcl lock clear-all-pins
zcl lock set-user-status [userId:2] [userStatus:1]
zcl lock get-user-status [userId:2]
zcl lock set-weekday-schedule [scheduleId:1] [userId:2] [daysMask:1] [startHour:1] [startMinute:1] [endHour:1] [endMinute:1]
zcl lock get-weekday-schedule [scheduleId:1] [userId:2]
zcl lock clear-weekday-schedule [scheduleId:1] [userId:2]
zcl lock set-yearday-schedule [scheduleId:1] [userId:2] [localStartTime:4] [localEndTime:4]
zcl lock get-yearday-schedule [scheduleId:1] [userId:2]
zcl lock clear-yearday-schedule [scheduleId:1] [userId:2]
zcl lock set-holiday-schedule [scheduleId:1] [localStartTime:4] [localEndTime:4] [operatingModeDuringHoliday:1]
zcl lock get-holiday-schedule [scheduleId:1]
zcl lock clear-holiday-schedule [scheduleId:1]
zcl lock set-user-type [userId:2] [userType:1]
zcl lock get-user-type [userId:2]
zcl lock set-rfid [userId:2] [userStatus:1] [userType:1] [id:-1]
zcl lock get-rfid [userId:2]
zcl lock clear-rfid [userId:2]
zcl lock clear-all-rfids
zcl lock set-disposable-schedule [userId:2] [localStartTime:4] [localEndTime:4]
zcl lock get-disposable-schedule [userId:2]
zcl lock clear-disposable-schedule [userId:2]
zcl lock clear-biometric-credential [userId:2]
zcl lock clear-all-biometric-credentials
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_LOCK#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_LOCK
zcl lock lock [PIN:-1]
Locks the door
PIN - CHAR_STRING
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_UNLOCK#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_UNLOCK
zcl lock unlock [PIN:-1]
Unlocks the door
PIN - CHAR_STRING
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_TOGGLE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_TOGGLE
zcl lock toggle [pin:-1]
Toggles the door lock from its current state to the opposite state locked or unlocked.
pin - CHAR_STRING
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_UNLOCK_WITH_TIMEOUT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_UNLOCK_WITH_TIMEOUT
zcl lock unlock-with-timeout [timeoutInSeconds:2] [pin:-1]
Unlock the door with a timeout. When the timeout expires, the door will automatically re-lock.
timeoutInSeconds - INT16U
pin - CHAR_STRING
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_LOG_RECORD#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_LOG_RECORD
zcl lock get-log-record [logIndex:2]
Retrieve a log record at a specified index.
logIndex - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_PIN#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_PIN
zcl lock set-pin [userId:2] [userStatus:1] [userType:1] [pin:-1]
Set the PIN for a specified user id.
userId - INT16U
userStatus - DoorLockUserStatus [ENUM8]
userType - DoorLockUserType [ENUM8]
pin - CHAR_STRING See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_PIN#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_PIN
zcl lock get-pin [userId:2]
Retrieve PIN information for a user with a specific user ID.
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_PIN#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_PIN
zcl lock clear-pin [userId:2]
Clear the PIN for a user with a specific user ID
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_ALL_PINS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_ALL_PINS
zcl lock clear-all-pins
Clear all PIN codes on the lock for all users.
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_USER_STATUS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_USER_STATUS
zcl lock set-user-status [userId:2] [userStatus:1]
Set the status value for a specified user ID.
userId - INT16U
userStatus - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_USER_STATUS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_USER_STATUS
zcl lock get-user-status [userId:2]
Retrieve the status byte for a specific user.
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_WEEKDAY_SCHEDULE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_WEEKDAY_SCHEDULE
zcl lock set-weekday-schedule [scheduleId:1] [userId:2] [daysMask:1] [startHour:1] [startMinute:1] [endHour:1] [endMinute:1]
Set the schedule of days during the week that the associated user based on the user ID will have access to the lock and will be able to operate it.
scheduleId - INT8U
userId - INT16U
daysMask - DoorLockDayOfWeek [BITMAP8]
startHour - INT8U
startMinute - INT8U
endHour - INT8U
endMinute - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_WEEKDAY_SCHEDULE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_WEEKDAY_SCHEDULE
zcl lock get-weekday-schedule [scheduleId:1] [userId:2]
Retrieve a weekday schedule for doorlock user activation for a specific schedule id and user id.
scheduleId - INT8U
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_WEEKDAY_SCHEDULE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_WEEKDAY_SCHEDULE
zcl lock clear-weekday-schedule [scheduleId:1] [userId:2]
Clear a weekday schedule for doorlock user activation for a specific schedule id and user id.
scheduleId - INT8U
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_YEARDAY_SCHEDULE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_YEARDAY_SCHEDULE
zcl lock set-yearday-schedule [scheduleId:1] [userId:2] [localStartTime:4] [localEndTime:4]
Set a door lock user id activation schedule according to a specific absolute local start and end time
scheduleId - INT8U
userId - INT16U
localStartTime - INT32U
localEndTime - INT32U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_YEARDAY_SCHEDULE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_YEARDAY_SCHEDULE
zcl lock get-yearday-schedule [scheduleId:1] [userId:2]
Retrieve a yearday schedule for a specific scheduleId and userId
scheduleId - INT8U
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_YEARDAY_SCHEDULE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_YEARDAY_SCHEDULE
zcl lock clear-yearday-schedule [scheduleId:1] [userId:2]
Clear a yearday schedule for a specific scheduleId and userId
scheduleId - INT8U
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_HOLIDAY_SCHEDULE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_HOLIDAY_SCHEDULE
zcl lock set-holiday-schedule [scheduleId:1] [localStartTime:4] [localEndTime:4] [operatingModeDuringHoliday:1]
Set the holiday schedule for a specific user
scheduleId - INT8U
localStartTime - INT32U
localEndTime - INT32U
operatingModeDuringHoliday - ENUM8
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_HOLIDAY_SCHEDULE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_HOLIDAY_SCHEDULE
zcl lock get-holiday-schedule [scheduleId:1]
Retrieve a holiday schedule for a specific scheduleId
scheduleId - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_HOLIDAY_SCHEDULE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_HOLIDAY_SCHEDULE
zcl lock clear-holiday-schedule [scheduleId:1]
Clear a holiday schedule for a specific scheduleId
scheduleId - INT8U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_USER_TYPE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_USER_TYPE
zcl lock set-user-type [userId:2] [userType:1]
Set the type value for a user based on user ID.
userId - INT16U
userType - DoorLockUserType [ENUM8] See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_USER_TYPE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_USER_TYPE
zcl lock get-user-type [userId:2]
Retrieve the type for a specific user based on the user ID.
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_RFID#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_RFID
zcl lock set-rfid [userId:2] [userStatus:1] [userType:1] [id:-1]
Set the PIN for a specified user id.
userId - INT16U
userStatus - DoorLockUserStatus [ENUM8]
userType - DoorLockUserType [ENUM8]
id - CHAR_STRING See Also
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_RFID#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_RFID
zcl lock get-rfid [userId:2]
Retrieve RFID ID information for a user with a specific user ID.
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_RFID#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_RFID
zcl lock clear-rfid [userId:2]
Clear the RFID ID for a user with a specific user ID
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_ALL_RFIDS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_ALL_RFIDS
zcl lock clear-all-rfids
Clear all RFID ID codes on the lock for all users.
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_DISPOSABLE_SCHEDULE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_SET_DISPOSABLE_SCHEDULE
zcl lock set-disposable-schedule [userId:2] [localStartTime:4] [localEndTime:4]
Set the Disposable Schedule by specifying local start time and local end time for the specific user.
userId - INT16U
localStartTime - INT32U
localEndTime - INT32U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_DISPOSABLE_SCHEDULE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_GET_DISPOSABLE_SCHEDULE
zcl lock get-disposable-schedule [userId:2]
Retrieve the disposable schedule for the specific user.
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_DISPOSABLE_SCHEDULE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_DISPOSABLE_SCHEDULE
zcl lock clear-disposable-schedule [userId:2]
Clear the Disposable schedule for the specific user
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_BIOMETRIC_CREDENTIAL#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_BIOMETRIC_CREDENTIAL
zcl lock clear-biometric-credential [userId:2]
Clear the Biometric Credential for the specific user
userId - INT16U
EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_ALL_BIOMETRIC_CREDENTIALS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_DOOR_LOCK_CLEAR_ALL_BIOMETRIC_CREDENTIALS
zcl lock clear-all-biometric-credentials
Clear out all Biometric Credentials on the lock