Cluster Commands: Generic Tunnel#
This group describes the CLI commands for the Generic Tunnel cluster. Listed below is a description of the cluster: The minimum common commands and attributes required to tunnel any protocol.
Macros#
zcl tunnel match [protocolAddress:-1]
zcl tunnel response [deviceIeeeAddress:8] [protocolAddress:-1]
zcl tunnel advertise [protocolAddress:-1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_GENERIC_TUNNEL_MATCH#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERIC_TUNNEL_MATCH
zcl tunnel match [protocolAddress:-1]
This command is generated when an application wishes to find the ZigBee address (node, endpoint) of the Generic Tunnel server cluster with a given ProtocolAddress attribute. The command is typically multicast to a group of inter-communicating Generic Tunnel clusters
protocolAddress - OCTET_STRING
EMBER_AF_DOXYGEN_CLI_COMMAND_GENERIC_TUNNEL_RESPONSE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERIC_TUNNEL_RESPONSE
zcl tunnel response [deviceIeeeAddress:8] [protocolAddress:-1]
This command is generated upon receipt of a Match Protocol Address command to indicate that the Protocol Address was successfully matched.
deviceIeeeAddress - IEEE_ADDRESS
protocolAddress - OCTET_STRING
EMBER_AF_DOXYGEN_CLI_COMMAND_GENERIC_TUNNEL_ADVERTISE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_GENERIC_TUNNEL_ADVERTISE
zcl tunnel advertise [protocolAddress:-1]
This command is typically sent upon startup, and whenever the ProtocolAddress attribute changes. It is typically multicast to a group of inter-communicating Generic Tunnel clusters.
protocolAddress - OCTET_STRING