Information discovered during a ZLL scan about the ZLL device's endpoint information.

Public Attributes#

EmberEUI64
uint8_t
uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

ieeeAddress#

EmberEUI64 EmberZllDeviceInfoRecord::ieeeAddress

Definition at line 151 of file stack/include/zll-types.h

endpointId#

uint8_t EmberZllDeviceInfoRecord::endpointId

Definition at line 152 of file stack/include/zll-types.h

profileId#

uint16_t EmberZllDeviceInfoRecord::profileId

Definition at line 153 of file stack/include/zll-types.h

deviceId#

uint16_t EmberZllDeviceInfoRecord::deviceId

Definition at line 154 of file stack/include/zll-types.h

version#

uint8_t EmberZllDeviceInfoRecord::version

Definition at line 155 of file stack/include/zll-types.h

groupIdCount#

uint8_t EmberZllDeviceInfoRecord::groupIdCount

Definition at line 156 of file stack/include/zll-types.h