Cluster Commands: Power Profile#
This group describes the CLI commands for the Power Profile cluster. Listed below is a description of the cluster:
 This cluster provides an interface for transferring power profile information from a device (e.g. Whitegood) to a controller (e.g. the Home Gateway). The Power Profile transferred can be solicited by client side (request command) or can be notified directly from the device (server side).
Macros#
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_POWER_PROFILE_PROFILE 
zcl power-profile profile [powerProfileId:1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_POWER_PROFILE_STATE 
zcl power-profile state
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_POWER_PROFILE_ENERGY_PHASES_SCHEDULE 
zcl power-profile energy-phases-schedule [powerProfileId:1] [numOfScheduledPhases:1] [scheduledPhases:3]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_POWER_PROFILE_SCHEDULE_CONSTRAINTS 
zcl power-profile schedule-constraints [powerProfileId:1]
#define
EMBER_AF_DOXYGEN_CLI_COMMAND_POWER_PROFILE_ENERGY_PHASES_SCHEDULE_STATES 
zcl power-profile energy-phases-schedule-states [powerProfileId:1]