Calendar Server#

Callbacks for Calendar Server Component.

Callbacks#

void
sl_zigbee_af_calendar_server_publish_info_cb(uint8_t publishCommandId, sl_802154_short_addr_t clientNodeId, uint8_t clientEndpoint, uint8_t totalCommands)

Publish information.

Callbacks Documentation#

sl_zigbee_af_calendar_server_publish_info_cb#

void sl_zigbee_af_calendar_server_publish_info_cb (uint8_t publishCommandId, sl_802154_short_addr_t clientNodeId, uint8_t clientEndpoint, uint8_t totalCommands)

Publish information.

Parameters
N/ApublishCommandId

ZCL command to be published Ver.: always

N/AclientNodeId

Destination nodeId Ver.: always

N/AclientEndpoint

Destination endpoint Ver.: always

N/AtotalCommands

Total number of publish commands to be sent Ver.: always

This function is called by the calendar-server plugin after receiving any of the following commands and just before it starts publishing the response: GetCalendar, GetDayProfiles, GetSeasons, GetSpecialDays, and GetWeekProfiles.


Definition at line 170 of file app/framework/plugin/calendar-server/calendar-server.h