Map actual endpoint type onto a specific endpoint.

Public Attribute Documentation#

endpoint#

uint8_t sl_zigbee_af_defined_endpoint_t::endpoint

Actual Zigbee endpoint number.


Definition at line 533 of file app/framework/include/af-types.h

profileId#

sl_zigbee_af_profile_id_t sl_zigbee_af_defined_endpoint_t::profileId

Profile ID of the device on this endpoint.


Definition at line 537 of file app/framework/include/af-types.h

deviceId#

uint16_t sl_zigbee_af_defined_endpoint_t::deviceId

Device ID of the device on this endpoint.


Definition at line 541 of file app/framework/include/af-types.h

deviceVersion#

uint8_t sl_zigbee_af_defined_endpoint_t::deviceVersion

Version of the device.


Definition at line 545 of file app/framework/include/af-types.h

endpointType#

sl_zigbee_af_endpoint_type_t* sl_zigbee_af_defined_endpoint_t::endpointType

Endpoint type for this endpoint.


Definition at line 549 of file app/framework/include/af-types.h

networkIndex#

uint8_t sl_zigbee_af_defined_endpoint_t::networkIndex

Network index for this endpoint.


Definition at line 553 of file app/framework/include/af-types.h

bitmask#

sl_zigbee_af_endpoint_bitmask_t sl_zigbee_af_defined_endpoint_t::bitmask

Meta-data about the endpoint.


Definition at line 557 of file app/framework/include/af-types.h