The sl_zigbee_af_message_struct_t is a struct wrapper that contains all the data about a low-level message to be sent (it may be ZCL or may be some other protocol).

Public Attributes#

sl_zigbee_aps_frame_t *
uint8_t *
sl_zigbee_outgoing_message_type_t

Public Attribute Documentation#

callback#

sl_zigbee_af_message_sent_function_t sl_zigbee_af_message_struct_t::callback

Definition at line 1512 of file app/framework/include/af-types.h

apsFrame#

sl_zigbee_aps_frame_t* sl_zigbee_af_message_struct_t::apsFrame

Definition at line 1513 of file app/framework/include/af-types.h

message#

uint8_t* sl_zigbee_af_message_struct_t::message

Definition at line 1514 of file app/framework/include/af-types.h

indexOrDestination#

uint16_t sl_zigbee_af_message_struct_t::indexOrDestination

Definition at line 1515 of file app/framework/include/af-types.h

messageLength#

uint16_t sl_zigbee_af_message_struct_t::messageLength

Definition at line 1516 of file app/framework/include/af-types.h

type#

sl_zigbee_outgoing_message_type_t sl_zigbee_af_message_struct_t::type

Definition at line 1517 of file app/framework/include/af-types.h

broadcast#

bool sl_zigbee_af_message_struct_t::broadcast

Definition at line 1518 of file app/framework/include/af-types.h