Contain basic information about an endpoint.

Public Attribute Documentation#

clusters#

sl_zigbee_af_cluster_info_t sl_zigbee_af_endpoint_info_struct_t::clusters[SL_ZIGBEE_AF_MAX_CLUSTERS_PER_ENDPOINT]

Definition at line 1905 of file app/framework/include/af-types.h

profileId#

sl_zigbee_af_profile_id_t sl_zigbee_af_endpoint_info_struct_t::profileId

Definition at line 1906 of file app/framework/include/af-types.h

deviceId#

uint16_t sl_zigbee_af_endpoint_info_struct_t::deviceId

Definition at line 1907 of file app/framework/include/af-types.h

endpoint#

uint8_t sl_zigbee_af_endpoint_info_struct_t::endpoint

Definition at line 1908 of file app/framework/include/af-types.h

clusterCount#

uint8_t sl_zigbee_af_endpoint_info_struct_t::clusterCount

Definition at line 1909 of file app/framework/include/af-types.h