Zigbee Internet Client/Server Remote Binding struct.

Public Attributes#

sl_802154_long_addr_t
uint16_t
sl_802154_long_addr_t
sl_802154_long_addr_t

Public Attribute Documentation#

targetEUI64#

sl_802154_long_addr_t sl_zigbee_af_remote_binding_struct_t::targetEUI64

Definition at line 1882 of file app/framework/include/af-types.h

sourceEndpoint#

uint8_t sl_zigbee_af_remote_binding_struct_t::sourceEndpoint

Definition at line 1883 of file app/framework/include/af-types.h

destEndpoint#

uint8_t sl_zigbee_af_remote_binding_struct_t::destEndpoint

Definition at line 1884 of file app/framework/include/af-types.h

clusterId#

uint16_t sl_zigbee_af_remote_binding_struct_t::clusterId

Definition at line 1885 of file app/framework/include/af-types.h

destEUI64#

sl_802154_long_addr_t sl_zigbee_af_remote_binding_struct_t::destEUI64

Definition at line 1886 of file app/framework/include/af-types.h

sourceEUI64#

sl_802154_long_addr_t sl_zigbee_af_remote_binding_struct_t::sourceEUI64

Definition at line 1887 of file app/framework/include/af-types.h