Describe clusters that are on the endpoint.

Public Attribute Documentation#

cluster#

sl_zigbee_af_cluster_t* sl_zigbee_af_endpoint_type_t::cluster

Pointer to the cluster structs, describing clusters on this endpoint type.


Definition at line 453 of file app/framework/include/af-types.h

clusterCount#

uint8_t sl_zigbee_af_endpoint_type_t::clusterCount

Number of clusters in this endpoint type.


Definition at line 457 of file app/framework/include/af-types.h

endpointSize#

uint16_t sl_zigbee_af_endpoint_type_t::endpointSize

Size of all non-external, non-singlet attribute, in this endpoint type.


Definition at line 461 of file app/framework/include/af-types.h