@ brief Struct used to specify priorities for Zigbee radio operations in multiprotocol

Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

backgroundRx#

uint8_t sl_zigbee_multiprotocol_priorities_t::backgroundRx

The priority of a Zigbee RX operation while not receiving a packet.


Definition at line 1709 of file stack/include/sl_zigbee_types.h

tx#

uint8_t sl_zigbee_multiprotocol_priorities_t::tx

The priority of a Zigbee TX operation.


Definition at line 1711 of file stack/include/sl_zigbee_types.h

activeRx#

uint8_t sl_zigbee_multiprotocol_priorities_t::activeRx

The priority of a Zigbee RX operation while receiving a packet.


Definition at line 1713 of file stack/include/sl_zigbee_types.h