Defines a ZigBee network and the associated parameters.

Public Attributes#

uint16_t
uint8_t

Public Attribute Documentation#

panId#

uint16_t sl_zigbee_zigbee_network_t::panId

channel#

uint8_t sl_zigbee_zigbee_network_t::channel

allowingJoin#

bool sl_zigbee_zigbee_network_t::allowingJoin

extendedPanId#

uint8_t sl_zigbee_zigbee_network_t::extendedPanId[EXTENDED_PAN_ID_SIZE]

stackProfile#

uint8_t sl_zigbee_zigbee_network_t::stackProfile

nwkUpdateId#

uint8_t sl_zigbee_zigbee_network_t::nwkUpdateId