A structure containing, per device, overall duty cycle consumed (up to the suspend limit).

Public Attributes#

sl_802154_short_addr_t

Public Attribute Documentation#

nodeId#

sl_802154_short_addr_t sl_zigbee_per_device_duty_cycle_t::nodeId

Node ID of the device whose duty cycle is reported.


Definition at line 2669 of file stack/include/sl_zigbee_types.h

dutyCycleConsumed#

sl_zigbee_duty_cycle_hecto_pct_t sl_zigbee_per_device_duty_cycle_t::dutyCycleConsumed

The amount of overall duty cycle consumed (up to suspend limit).


Definition at line 2671 of file stack/include/sl_zigbee_types.h