Public Attribute Documentation#

allocateMemoryForResponses#

bool sl_zigbee_af_gbz_message_creator_state_t::allocateMemoryForResponses

command#

uint8_t* sl_zigbee_af_gbz_message_creator_state_t::command

commandIndex#

uint16_t sl_zigbee_af_gbz_message_creator_state_t::commandIndex

commandLength#

uint16_t sl_zigbee_af_gbz_message_creator_state_t::commandLength

responses#

sli_zigbee_af_gbz_use_case_specific_component* sl_zigbee_af_gbz_message_creator_state_t::responses

lastResponse#

sli_zigbee_af_gbz_use_case_specific_component* sl_zigbee_af_gbz_message_creator_state_t::lastResponse

header#

sli_zigbee_af_gbz_payload_header* sl_zigbee_af_gbz_message_creator_state_t::header

nextEncryptedComponentZclSequenceNumber#

uint8_t sl_zigbee_af_gbz_message_creator_state_t::nextEncryptedComponentZclSequenceNumber

nextComponentZclSequenceNumber#

uint8_t sl_zigbee_af_gbz_message_creator_state_t::nextComponentZclSequenceNumber

nextAdditionalHeaderFrameCounter#

uint8_t sl_zigbee_af_gbz_message_creator_state_t::nextAdditionalHeaderFrameCounter

componentsCount#

uint8_t* sl_zigbee_af_gbz_message_creator_state_t::componentsCount

lastExtHeaderControlField#

uint8_t* sl_zigbee_af_gbz_message_creator_state_t::lastExtHeaderControlField

messageCode#

uint16_t sl_zigbee_af_gbz_message_creator_state_t::messageCode

result#

sl_zigbee_af_gbz_message_creator_result_t sl_zigbee_af_gbz_message_creator_state_t::result