The information regarding scan results.
Public Attribute Documentation#
status#
sl_status_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::status
The status indicating the success or failure of a scan.
This member is only valid when sl_zigbee_af_scan_dispatch_scan_results_are_complete returns true.
rssi#
int8_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::rssi
The RSSI found during a scan.
This member is only valid when sl_zigbee_af_scan_dispatch_scan_results_are_complete returns false.
channel#
uint8_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::channel
The channel on which the scan is taking place.
This member is only valid when the results are for an energy scan or sl_zigbee_af_scan_dispatch_scan_results_are_complete returns true and sl_zigbee_af_scan_dispatch_scan_results_are_failure returns false. Note that in active scan results, users can find the channel on which the network was found using the network member of this structure.
lqi#
uint8_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::lqi
The LQI found during the scan.
This member is only valid when the result are for an active scan.
network#
sl_zigbee_zigbee_network_t* sl_zigbee_af_plugin_scan_dispatch_scan_results_t::network
The Zigbee network found in the scan.
This member is only valid when the result are for an active scan.
mask#
uint16_t sl_zigbee_af_plugin_scan_dispatch_scan_results_t::mask
A mask containing information about the scan.