Basic#
Callbacks for Basic Component.
Callbacks#
void
sl_zigbee_af_basic_reset_to_factory_defaults_cb(uint8_t endpoint)
Reset to factory defaults.
Callbacks Documentation#
sl_zigbee_af_basic_reset_to_factory_defaults_cb#
void sl_zigbee_af_basic_reset_to_factory_defaults_cb (uint8_t endpoint)
Reset to factory defaults.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | endpoint | Ver.: always  | 
This function is called by the Basic server plugin when a request to reset to factory defaults is received. The plugin resets attributes managed by the framework to their default values. The application should perform any other necessary reset-related operations in this callback, including resetting any externally-stored attributes.