Color Control Server#
Callbacks for Color Control Server Component.
Callbacks#
void
sl_zigbee_af_color_control_server_compute_pwm_from_hsv_cb(uint8_t endpoint)
Compute PWM from HSV.
void
sl_zigbee_af_color_control_server_compute_pwm_from_xy_cb(uint8_t endpoint)
Compute PWM from HSV.
void
sl_zigbee_af_color_control_server_compute_pwm_from_temp_cb(uint8_t endpoint)
Compute PWM from HSV.
Callbacks Documentation#
sl_zigbee_af_color_control_server_compute_pwm_from_hsv_cb#
void sl_zigbee_af_color_control_server_compute_pwm_from_hsv_cb (uint8_t endpoint)
Compute PWM from HSV.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | endpoint | The identifying endpoint Ver.: always  | 
This function is called from the color server when the PWMs need to be driven with a new value from the HSV values.
sl_zigbee_af_color_control_server_compute_pwm_from_xy_cb#
void sl_zigbee_af_color_control_server_compute_pwm_from_xy_cb (uint8_t endpoint)
Compute PWM from HSV.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | endpoint | The identifying endpoint Ver.: always  | 
This function is called from the color server when the PWMs need to be driven with a new value from the color X and color Y values.
sl_zigbee_af_color_control_server_compute_pwm_from_temp_cb#
void sl_zigbee_af_color_control_server_compute_pwm_from_temp_cb (uint8_t endpoint)
Compute PWM from HSV.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | endpoint | The identifying endpoint Ver.: always  | 
This function is called from the color server when the PWMs need to be driven with a new value from the color temperature.