WWAH App Event Retry Manager#
API and Callbacks for the WWAH App Event Retry Manager Component.
Silicon Labs proprietary Works With All Hubs (WWAH) app event retry manager.
Modules#
API#
Write attribute-enabled callback.
Write attribute queue size callback.
WWAH app event retry manager set backoff parameters to default.
API Documentation#
sl_zigbee_af_wwah_app_event_retry_manager_write_attribute_enabled#
void sl_zigbee_af_wwah_app_event_retry_manager_write_attribute_enabled (uint8_t enabled)
Write attribute-enabled callback.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | enabled | Ver.: always  | 
This callback is called when the enabled backoff parameter is changed.
sl_zigbee_af_wwah_app_event_retry_manager_write_attribute_queue_size#
void sl_zigbee_af_wwah_app_event_retry_manager_write_attribute_queue_size (uint8_t queueSize)
Write attribute queue size callback.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | queueSize | Ver.: always  | 
This callback is called when the app event retry queue size is being reported.
sl_zigbee_af_wwah_app_event_retry_manager_set_backoff_params_to_default#
void sl_zigbee_af_wwah_app_event_retry_manager_set_backoff_params_to_default (void )
WWAH app event retry manager set backoff parameters to default.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
This callback is called when the app event retry manager is about to set the backoff parameters of the critical message queue provider plugin back to their default.