Gas Proxy Function#
API and Callbacks for the Gas Proxy Function Component.
Silicon Labs implementation of the Gas Proxy Function (GPF). This component receives and processes GBZ Top Off Messages. NOTE: This component uses malloc and should only be used in a non-SoC setup.
Modules#
Handlers#
API#
Ignore future commands. Per GBCS v0.8.1, section 10.3.4.2 Step 12/13, it is inferred that per elemental ZCL command, future commands ( startTime greater than now ) will be discarded and the application will be notified.
Handlers Documentation#
sl_zigbee_af_gas_proxy_function_non_tap_off_message_handler#
sl_status_t sl_zigbee_af_gas_proxy_function_non_tap_off_message_handler (uint8_t * gbzCommands, uint16_t gbzCommandsLength, uint16_t messageCode)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t * | N/A | gbzCommands | |
| uint16_t | N/A | gbzCommandsLength | |
| uint16_t | N/A | messageCode | 
sl_zigbee_af_gas_proxy_function_tap_off_message_handler#
sl_status_t sl_zigbee_af_gas_proxy_function_tap_off_message_handler (uint8_t * gbzCommand, uint16_t gbzCommandLength, uint8_t * gbzCommandResponse, uint16_t gbzCommandResponseLength, uint16_t messageCode)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t * | N/A | gbzCommand | |
| uint16_t | N/A | gbzCommandLength | |
| uint8_t * | N/A | gbzCommandResponse | |
| uint16_t | N/A | gbzCommandResponseLength | |
| uint16_t | N/A | messageCode | 
API Documentation#
sl_zigbee_af_gas_proxy_function_ignore_future_command#
bool sl_zigbee_af_gas_proxy_function_ignore_future_command (uint32_t startTime)
Ignore future commands. Per GBCS v0.8.1, section 10.3.4.2 Step 12/13, it is inferred that per elemental ZCL command, future commands ( startTime greater than now ) will be discarded and the application will be notified.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | N/A | startTime | 
Returns
true - if future dated current command are ignored, false - otherwise.