End Device Support#
API and Callbacks for the End Device Support Component.
Silicon Labs implementation of polling for end devices. Note that the Poll Control Server component sets the long and short poll intervals at startup. If both components are enabled, the long and short poll intervals set here will not be used.
Modules#
Handlers#
void
sl_zigbee_af_end_device_support_move_network_event_handler(sl_zigbee_af_event_t *event)
Handlers Documentation#
sl_zigbee_af_end_device_support_move_network_event_handler#
void sl_zigbee_af_end_device_support_move_network_event_handler (sl_zigbee_af_event_t * event)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_zigbee_af_event_t * | N/A | event |