Device Query Service#
API and Callbacks for the Device Query Service Component.
This component queries new devices for their endpoints and clusters to record information in the Device Database component.
API#
void
sl_zigbee_af_device_query_service_enable_disable(bool enable)
Enable / disable the device query service.
bool
Device query service get state.
void
sl_zigbee_af_device_query_service_get_current_discovery_target_eui64(sl_802154_long_addr_t returnEui64)
Get EUI64 of current discovery target.
API Documentation#
sl_zigbee_af_device_query_service_enable_disable#
void sl_zigbee_af_device_query_service_enable_disable (bool enable)
Enable / disable the device query service.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| bool | N/A | enable | enable/disbale value Ver.:Always  | 
sl_zigbee_af_device_query_service_get_enabled_state#
bool sl_zigbee_af_device_query_service_get_enabled_state (void )
Device query service get state.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Returns
enable state
sl_zigbee_af_device_query_service_get_current_discovery_target_eui64#
void sl_zigbee_af_device_query_service_get_current_discovery_target_eui64 (sl_802154_long_addr_t returnEui64)
Get EUI64 of current discovery target.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_802154_long_addr_t | N/A | returnEui64 | Ver.:Always  |