Find and Bind Initiator#
API and Callbacks for the Find and Bind Initiator Component.
This component provides the functionality to find devices that are performing the find and bind process for a target and then optionally attempts to create a binding to those devices.
Modules#
API#
sl_zigbee_af_find_and_bind_initiator_start(uint8_t endpoint)
Start initiator finding and binding operations.
Macros#
#define
SL_ZIGBEE_AF_PLUGIN_FIND_AND_BIND_INITIATOR_PLUGIN_NAME "Find and Bind Initiator"
API Documentation#
sl_zigbee_af_find_and_bind_initiator_start#
sl_status_t sl_zigbee_af_find_and_bind_initiator_start (uint8_t endpoint)
Start initiator finding and binding operations.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | endpoint | The endpoint on which to begin initiator operations.  | 
A call to this function will commence the initiator finding and binding operations. Specifically, the initiator will attempt to start searching for potential bindings that can be made with identifying targets.
Returns
An sl_status_t value describing the success of the commencement of the initiator operations.