Level Control Server#
API and Callbacks for the Level Control Cluster Server Component.
Silicon Labs implementation of the Level Control server cluster. If the ZLL Level Control server cluster component is also enabled, this component uses it to handle ZLL enhancements. Otherwise, all ZLL extensions are disabled. It is not intended for production but provides sample code to show how the cluster could be implemented.
This group describes the CLI commands for the Level Control cluster. Listed below is a description of the cluster:
 Attributes and commands for controlling devices that can be set to a level between fully 'On' and fully 'Off.'
Modules#
Macros#
zcl level-control mv-to-level [level:1] [transitionTime:2] [optionMask:1] [optionOverride:1]
zcl level-control move [moveMode:1] [rate:1] [optionMask:1] [optionOverride:1]
zcl level-control step [stepMode:1] [stepSize:1] [transitionTime:2] [optionMask:1] [optionOverride:1]
zcl level-control stop [optionMask:1] [optionOverride:1]
zcl level-control o-mv-to-level [level:1] [transitionTime:2]
zcl level-control o-move [moveMode:1] [rate:1]
zcl level-control o-step [stepMode:1] [stepSize:1] [transitionTime:2]
zcl level-control o-stop
zcl level-control mv-to-closest-freq [frequency:2]