Prepayment Server#
Callbacks for Prepayment Server Component.
Callbacks#
Prepayment Cluster Server Attribute Changed.
Prepayment cluster server default response.
Initialize the prepayment cluster server.
Prepayment cluster server manufacturer-specific attribute changed.
Prepayment cluster server message sent.
Prepayment cluster server pre attribute changed.
Callbacks Documentation#
sl_zigbee_af_prepayment_cluster_server_attribute_changed_cb#
void sl_zigbee_af_prepayment_cluster_server_attribute_changed_cb (uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId)
Prepayment Cluster Server Attribute Changed.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | endpoint | Endpoint that is being initialized Ver.: always  | 
| sl_zigbee_af_attribute_id_t | N/A | attributeId | Attribute that changed Ver.: always  | 
sl_zigbee_af_prepayment_cluster_server_default_response_cb#
void sl_zigbee_af_prepayment_cluster_server_default_response_cb (uint8_t endpoint, uint8_t commandId, sl_zigbee_af_status_t status)
Prepayment cluster server default response.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | endpoint | Destination endpoint Ver.: always  | 
| uint8_t | N/A | commandId | Command id Ver.: always  | 
| sl_zigbee_af_status_t | N/A | status | Status in default response Ver.: always  | 
This function is called when the server receives the default response from the client.
sl_zigbee_af_prepayment_cluster_server_init_cb#
void sl_zigbee_af_prepayment_cluster_server_init_cb (uint8_t endpoint)
Initialize the prepayment cluster server.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | endpoint | Endpoint that is being initialized Ver.: always  | 
sl_zigbee_af_prepayment_cluster_server_manufacturer_specific_attribute_changed_cb#
void sl_zigbee_af_prepayment_cluster_server_manufacturer_specific_attribute_changed_cb (uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId, uint16_t manufacturerCode)
Prepayment cluster server manufacturer-specific attribute changed.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | endpoint | Endpoint that is being initialized Ver.: always  | 
| sl_zigbee_af_attribute_id_t | N/A | attributeId | Attribute that changed Ver.: always  | 
| uint16_t | N/A | manufacturerCode | Manufacturer Code of the attribute that changed Ver.: always  | 
sl_zigbee_af_prepayment_cluster_server_message_sent_cb#
void sl_zigbee_af_prepayment_cluster_server_message_sent_cb (sl_zigbee_outgoing_message_type_t type, uint16_t indexOrDestination, sl_zigbee_aps_frame_t * apsFrame, uint16_t msgLen, uint8_t * message, sl_status_t status)
Prepayment cluster server message sent.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_zigbee_outgoing_message_type_t | N/A | type | The type of message sent Ver.: always  | 
| uint16_t | N/A | indexOrDestination | The destination or address to which the message was sent Ver.: always  | 
| sl_zigbee_aps_frame_t * | N/A | apsFrame | The APS frame for the message Ver.: always  | 
| uint16_t | N/A | msgLen | The length of the message Ver.: always  | 
| uint8_t * | N/A | message | The message that was sent Ver.: always  | 
| sl_status_t | N/A | status | The status of the sent message Ver.: always  | 
sl_zigbee_af_prepayment_cluster_server_pre_attribute_changed_cb#
sl_zigbee_af_status_t sl_zigbee_af_prepayment_cluster_server_pre_attribute_changed_cb (uint8_t endpoint, sl_zigbee_af_attribute_id_t attributeId, sl_zigbee_af_attribute_type_t attributeType, uint8_t size, uint8_t * value)
Prepayment cluster server pre attribute changed.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | endpoint | Endpoint that is being initialized Ver.: always  | 
| sl_zigbee_af_attribute_id_t | N/A | attributeId | Attribute to be changed Ver.: always  | 
| sl_zigbee_af_attribute_type_t | N/A | attributeType | Attribute type Ver.: always  | 
| uint8_t | N/A | size | Attribute size Ver.: always  | 
| uint8_t * | N/A | value | Attribute value Ver.: always  |