Simple Metering Client#
Callbacks for Simple Metering Client Component.
Callbacks#
uint16_t
sl_zigbee_af_simple_metering_client_request_mirror_cb(sl_802154_long_addr_t requestingDeviceIeeeAddress)
Request Mirror.
uint16_t
sl_zigbee_af_simple_metering_client_remove_mirror_cb(sl_802154_long_addr_t requestingDeviceIeeeAddress)
Remove Mirror.
Callbacks Documentation#
sl_zigbee_af_simple_metering_client_request_mirror_cb#
uint16_t sl_zigbee_af_simple_metering_client_request_mirror_cb (sl_802154_long_addr_t requestingDeviceIeeeAddress)
Request Mirror.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_802154_long_addr_t | N/A | requestingDeviceIeeeAddress | Ver.: always  | 
This function is called by the Simple Metering client plugin whenever a Request Mirror command is received. The application should return the endpoint to which the mirror has been assigned. If no mirror could be assigned, the application should return 0xFFFF.
sl_zigbee_af_simple_metering_client_remove_mirror_cb#
uint16_t sl_zigbee_af_simple_metering_client_remove_mirror_cb (sl_802154_long_addr_t requestingDeviceIeeeAddress)
Remove Mirror.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_802154_long_addr_t | N/A | requestingDeviceIeeeAddress | Ver.: always  | 
This function is called by the Simple Metering client plugin whenever a Remove Mirror command is received. The application should return the endpoint on which the mirror has been removed. If the mirror could not be removed, the application should return 0xFFFF.