WWAH Client Silicon Labs#
Callbacks for WWAH Client Silicon Labs Component.
Callbacks#
void
sl_zigbee_af_sl_wwah_cluster_client_init_cb(uint8_t endpoint)
WWAH cluster client init callback.
bool
sl_zigbee_af_sl_wwah_cluster_debug_report_query_response_cb(uint8_t debugReportId, uint8_t *debugReportData)
WWAH cluster debug report query response callback.
Callbacks Documentation#
sl_zigbee_af_sl_wwah_cluster_client_init_cb#
void sl_zigbee_af_sl_wwah_cluster_client_init_cb (uint8_t endpoint)
WWAH cluster client init callback.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | endpoint | end point  | 
sl_zigbee_af_sl_wwah_cluster_debug_report_query_response_cb#
bool sl_zigbee_af_sl_wwah_cluster_debug_report_query_response_cb (uint8_t debugReportId, uint8_t * debugReportData)
WWAH cluster debug report query response callback.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | N/A | debugReportId | debug report ID  | 
| uint8_t * | N/A | debugReportData | debug report data  |