Edit

Using the Gecko Bootloader with EmberZNet#

Note: This section replaces AN1084: Using the Gecko Bootloader with EmberZNet. Further updates to this application note will be provided here.

This application note includes detailed information on using the Silicon Labs Gecko Bootloader with EmberZNet. It supplements the general Gecko Bootloader implementation information provided in Gecko Bootloader User's Guide for Series 3, Silicon Labs Gecko Bootloader User's Guide for GSDK 4.0 and Higher, or UG266: Silicon Labs Gecko Bootloader User’s Guide for GSDK 3.2 and Lower. If you are not familiar with the basic principles of performing a firmware upgrade or want more information about upgrading image files, refer to Bootloader Fundamentals.

Key Points#

  • Gecko Bootloader overview.

  • Using Gecko standalone bootloaders.

  • Using Gecko application bootloaders.