You are viewing documentation for version:
Sidewalk Phy settings to configure radio prior to transmission and reception.
Public Attribute Documentation#
data_rate#
sid_pal_radio_data_rate_t sid_pal_radio_packet_cfg_t::data_rate
Data rate for the packet
channel#
uint8_t sid_pal_radio_packet_cfg_t::channel
Channel on which the packet will be transmitted or received
invert_IQ#
uint8_t sid_pal_radio_packet_cfg_t::invert_IQ
Flag to indicate if IQ inversion is enabled
preamble_len#
uint16_t sid_pal_radio_packet_cfg_t::preamble_len
Length of the preamble
symbol_timeout#
uint32_t sid_pal_radio_packet_cfg_t::symbol_timeout
Symbol timeout value
crc_enabled#
bool sid_pal_radio_packet_cfg_t::crc_enabled
Flag to indicate if CRC is enabled