Sidewalk Phy transmit packet configuration.

Public Attribute Documentation#

packet_cfg#

sid_pal_radio_packet_cfg_t sid_pal_radio_tx_packet_t::packet_cfg

Configuration for the packet


tx_power_in_dbm#

int8_t sid_pal_radio_tx_packet_t::tx_power_in_dbm

Transmit power in dBm


tx_payload#

uint8_t* sid_pal_radio_tx_packet_t::tx_payload

Pointer to the payload to be transmitted


payload_len#

uint8_t sid_pal_radio_tx_packet_t::payload_len

Length of the payload


timeout#

uint32_t sid_pal_radio_tx_packet_t::timeout

Timeout for the transmission