Data structure of the notification_tx_completed event.

Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_gatt_server_notification_tx_completed_s::connection

Connection handle


Definition at line 9613 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

count#

uint8_t sl_bt_evt_gatt_server_notification_tx_completed_s::count

Number of notifications that have been transmitted


Definition at line 9614 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h