You are viewing documentation for version:
Data structure of the passkey_display event. 
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_sm_passkey_display_s::connection
Connection handle 
passkey#
uint32_t sl_bt_evt_sm_passkey_display_s::passkey
Passkey. Range: 0 to 999999.
- NOTE! When displaying the passkey to the user, prefix the number with zeros to obtain a 6 digit number 
- Example: Passkey value is 42 
- Number to display to the user is 000042