GATT Characteristic Property Flags#
This enum defines the property flags for GATT characteristic values. Lower byte is Characteristic Properties and higher byte is Characteristic Extended Properties.
Macro Definition Documentation#
SL_BT_GATTDB_CHARACTERISTIC_READ#
#define SL_BT_GATTDB_CHARACTERISTIC_READValue:
0x2
A GATT client can read the characteristic value.
Definition at line
8760
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
SL_BT_GATTDB_CHARACTERISTIC_WRITE_NO_RESPONSE#
#define SL_BT_GATTDB_CHARACTERISTIC_WRITE_NO_RESPONSEValue:
0x4
A GATT client can write the characteristic value without a response.
Definition at line
8763
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
SL_BT_GATTDB_CHARACTERISTIC_WRITE#
#define SL_BT_GATTDB_CHARACTERISTIC_WRITEValue:
0x8
A GATT client can write the characteristic value.
Definition at line
8766
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
SL_BT_GATTDB_CHARACTERISTIC_NOTIFY#
#define SL_BT_GATTDB_CHARACTERISTIC_NOTIFYValue:
0x10
The characteristic value can be notified without acknowledgment.
Definition at line
8769
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
SL_BT_GATTDB_CHARACTERISTIC_INDICATE#
#define SL_BT_GATTDB_CHARACTERISTIC_INDICATEValue:
0x20
The characteristic value can be notified with acknowledgment.
Definition at line
8772
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
SL_BT_GATTDB_CHARACTERISTIC_EXTENDED_PROPS#
#define SL_BT_GATTDB_CHARACTERISTIC_EXTENDED_PROPSValue:
0x80
The additional characteristic properties are defined.
Definition at line
8775
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h
SL_BT_GATTDB_CHARACTERISTIC_RELIABLE_WRITE#
#define SL_BT_GATTDB_CHARACTERISTIC_RELIABLE_WRITEValue:
0x101
The characteristic value supports reliable write.
Definition at line
8778
of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h