GATT Database Flags#

This enum defines the options of GATT attribute management.

Macro Definition Documentation#

SL_BT_GATTDB_NO_AUTO_CCCD#

#define SL_BT_GATTDB_NO_AUTO_CCCD
Value:
0x1

Do not automatically create a Client Characteristic Configuration descriptor when adding a characteristic that has the notify or indicate property.


Definition at line 8746 of file /mnt/raid/workspaces/ws.0zwF9W456/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h