Data structure of the remote_used_features event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_connection_remote_used_features_s::connection
Connection handle
Definition at line
6880
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
features#
uint8array sl_bt_evt_connection_remote_used_features_s::features
This parameter is 8 bytes in little endian format and contains bit fields describing the supported link layer features of the remote device. Bit value 1 means that the feature is supported.
The bits are explained in Bluetooth specification Vol 6, Part B, 4.6.
Definition at line
6881
of file /mnt/raid/workspaces/ws.XK183xwsq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h