Data structure of the extended_advertisement_report event.

Public Attribute Documentation#

event_flags#

uint8_t sl_bt_evt_scanner_extended_advertisement_report_s::event_flags

The event type flag(s) in the advertisement packet. Value: One or more flags defined in Event Type Flags of Advertisement Reports


address#

bd_addr sl_bt_evt_scanner_extended_advertisement_report_s::address

Advertiser address


address_type#

uint8_t sl_bt_evt_scanner_extended_advertisement_report_s::address_type

Enum sl_bt_gap_address_type_t.

Advertiser address type.

If the application does not include the bluetooth_feature_use_accurate_api_address_types component, address_type uses the following values:

  • 0: Public address

  • 1: Random address

  • 255: No address provided (anonymous advertising)

If the application includes the bluetooth_feature_use_accurate_api_address_types component, address_type uses enum sl_bt_gap_address_type_t values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address

  • sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address

  • sl_bt_gap_anonymous_address (0xff): No address provided (anonymous advertising)

  • sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)

  • sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)


bonding#

uint8_t sl_bt_evt_scanner_extended_advertisement_report_s::bonding

Bonding handle if the remote advertising device has previously bonded with the local device. Values:

  • SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding

  • Other: Bonding handle


rssi#

int8_t sl_bt_evt_scanner_extended_advertisement_report_s::rssi

Signal strength indicator (RSSI) in the last received packet. Units: dBm

  • Range: -127 to +20


channel#

uint8_t sl_bt_evt_scanner_extended_advertisement_report_s::channel

The channel number on which the last packet was received


target_address#

bd_addr sl_bt_evt_scanner_extended_advertisement_report_s::target_address

The target address if this is directed advertising, otherwise ignored


target_address_type#

uint8_t sl_bt_evt_scanner_extended_advertisement_report_s::target_address_type

Enum sl_bt_gap_address_type_t.

The target address type if the advertisement is from directed advertising, otherwise ignored.

If the application does not include the bluetooth_feature_use_accurate_api_address_types component, target_address_type uses the following values:

  • 0: Public address

  • 1: Random address

If the application includes the bluetooth_feature_use_accurate_api_address_types component, target_address_type uses enum sl_bt_gap_address_type_t values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address

  • sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address

  • sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)

  • sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)


adv_sid#

uint8_t sl_bt_evt_scanner_extended_advertisement_report_s::adv_sid

Advertising set identifier


primary_phy#

uint8_t sl_bt_evt_scanner_extended_advertisement_report_s::primary_phy

Enum sl_bt_gap_phy_t. The PHY on which advertising packets are transmitted on the primary advertising channel Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)


secondary_phy#

uint8_t sl_bt_evt_scanner_extended_advertisement_report_s::secondary_phy

Enum sl_bt_gap_phy_t. The PHY on which advertising packets are transmitted on the secondary advertising channel Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_2m (0x2): 2M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)


tx_power#

int8_t sl_bt_evt_scanner_extended_advertisement_report_s::tx_power

TX power value in the received packet header. Units: dBm

  • Valid value range: -127 to 126

  • Value 127: information unavailable


periodic_interval#

uint16_t sl_bt_evt_scanner_extended_advertisement_report_s::periodic_interval

The periodic advertising interval. Value 0 indicates no periodic advertising. Otherwise,

  • Range: 0x06 to 0xFFFF

  • Unit: 1.25 ms

  • Time range: 7.5 ms to 81.92 s


data_completeness#

uint8_t sl_bt_evt_scanner_extended_advertisement_report_s::data_completeness

Enum sl_bt_scanner_data_status_t. The data completeness status. Values:

  • sl_bt_scanner_data_status_complete (0x0): All data of the advertisement has been reported.

  • sl_bt_scanner_data_status_incomplete_more (0x1): Data of the advertisement is incomplete in this event, and more data will come in new events.

  • sl_bt_scanner_data_status_incomplete_nomore (0x2): Data of the advertisement is incomplete in this event, but no more data will come, i.e., the data of the advertisement is truncated.


counter#

uint8_t sl_bt_evt_scanner_extended_advertisement_report_s::counter

The monotonically increasing counter as the sequence number of the event. This counter is specific to sl_bt_evt_scanner_extended_advertisement_report_id. It can be used to detect if one more sl_bt_evt_scanner_extended_advertisement_report events were dropped due to temporarily out of resources or other reasons. Ignore this field if event loss is not a concern.


data#

uint8array sl_bt_evt_scanner_extended_advertisement_report_s::data

Advertising or scan response data