sl_bt_evt_scanner_scan_report#

Deprecated and replaced by new sl_bt_evt_scanner_legacy_advertisement_report and sl_bt_evt_scanner_extended_advertisement_report events

To use these new events, the application needs to include the bluetooth_feature_legacy_scanner or bluetooth_feature_extended_scanner component.

Reports an advertising or scan response packet from an advertising device that uses legacy or extended advertising PDUs.

Modules#

sl_bt_evt_scanner_scan_report_s

Macros#

#define

Identifier of the scan_report event.

Typedef Documentation#

sl_bt_evt_scanner_scan_report_t#

typedef struct sl_bt_evt_scanner_scan_report_s sl_bt_evt_scanner_scan_report_t

Definition at line 4251 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_scanner_scan_report_id#

#define sl_bt_evt_scanner_scan_report_id
Value:
0x010500a0

Identifier of the scan_report event.


Definition at line 4136 of file /mnt/raid/workspaces/ws.pY3F1RWXq/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h