Data structure of the scan_report event.

Public Attributes#

uint8_t
uint8_t
int8_t
int8_t
uint8_t

Public Attribute Documentation#

packet_type#

uint8_t sl_bt_evt_scanner_scan_report_s::packet_type

Bits 0..2 : advertising packet type

  • 000 : Connectable scannable undirected advertising

  • 001 : Connectable undirected advertising

  • 010 : Scannable undirected advertising

  • 011 : Non-connectable non-scannable undirected advertising

  • 100 : Scan Response. Note that this is received only if the device is in active scan mode.

Bits 3..4 : Reserved for future

Bits 5..6 : data completeness

  • 00: Complete

  • 01: Incomplete, more data to come in new events

  • 10: Incomplete, data truncated, no more to come

Bit 7 : legacy or extended advertising

  • 0: Legacy advertising PDUs used

  • 1: Extended advertising PDUs used


address#

bd_addr sl_bt_evt_scanner_scan_report_s::address

Bluetooth address of the remote device


address_type#

uint8_t sl_bt_evt_scanner_scan_report_s::address_type

Enum sl_bt_gap_address_type_t.

Advertiser address type.

If the application does not include the bluetooth_feature_use_accurate_api_address_types component, address_type uses the following values:

  • 0: Public address

  • 1: Random address

  • 255: No address provided (anonymous advertising)

If the application includes the bluetooth_feature_use_accurate_api_address_types component, address_type uses enum sl_bt_gap_address_type_t values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address

  • sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address

  • sl_bt_gap_anonymous_address (0xff): No address provided (anonymous advertising)

  • sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)

  • sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)


bonding#

uint8_t sl_bt_evt_scanner_scan_report_s::bonding

Bonding handle if the remote advertising device has previously bonded with the local device. Values:

  • SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding

  • Other: Bonding handle


primary_phy#

uint8_t sl_bt_evt_scanner_scan_report_s::primary_phy

Enum sl_bt_gap_phy_t. The PHY on which advertising packets are transmitted on the primary advertising channel. Ignore this field if the report is for a legacy advertising PDU. Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)


secondary_phy#

uint8_t sl_bt_evt_scanner_scan_report_s::secondary_phy

Enum sl_bt_gap_phy_t. The PHY on which advertising packets are transmitted on the secondary advertising channel. Ignore this field if the report is for a legacy advertising PDU. Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_2m (0x2): 2M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)


adv_sid#

uint8_t sl_bt_evt_scanner_scan_report_s::adv_sid

Advertising set identifier


tx_power#

int8_t sl_bt_evt_scanner_scan_report_s::tx_power

TX power value in the received packet header. Units: dBm

  • Valid value range: -127 to 126

  • Value 127: information unavailable


rssi#

int8_t sl_bt_evt_scanner_scan_report_s::rssi

Signal strength indicator (RSSI) in the last received packet. Units: dBm

  • Range: -127 to +20


channel#

uint8_t sl_bt_evt_scanner_scan_report_s::channel

The channel number on which the last packet was received


periodic_interval#

uint16_t sl_bt_evt_scanner_scan_report_s::periodic_interval

The periodic advertising interval. Value 0 indicates no periodic advertising. Otherwise,

  • Range: 0x06 to 0xFFFF

  • Unit: 1.25 ms

  • Time range: 7.5 ms to 81.92 s


data#

uint8array sl_bt_evt_scanner_scan_report_s::data

Advertising or scan response data