You are viewing documentation for version:
Data structure of the boot event. 
Public Attribute Documentation#
major#
uint16_t sl_bt_evt_system_boot_s::major
Major release version 
minor#
uint16_t sl_bt_evt_system_boot_s::minor
Minor release version 
patch#
uint16_t sl_bt_evt_system_boot_s::patch
Patch release number 
build#
uint16_t sl_bt_evt_system_boot_s::build
Build number 
bootloader#
uint32_t sl_bt_evt_system_boot_s::bootloader
Unused. Ignore this field. 
uint16_t sl_bt_evt_system_boot_s::hw
Hardware type: the major chip revision number in the most significant byte and the minor revision in the least significant byte 
hash#
uint32_t sl_bt_evt_system_boot_s::hash
Version hash