Data structure of the parameters event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_connection_parameters_s::connection
Connection handle
5599
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
interval#
uint16_t sl_bt_evt_connection_parameters_s::interval
Connection interval. Time = Value x 1.25 ms
5600
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
latency#
uint16_t sl_bt_evt_connection_parameters_s::latency
Peripheral latency (how many connection intervals the peripheral can skip)
5601
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
timeout#
uint16_t sl_bt_evt_connection_parameters_s::timeout
Supervision timeout. Time = Value x 10 ms
5603
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
security_mode#
uint8_t sl_bt_evt_connection_parameters_s::security_mode
Enum sl_bt_connection_security_t. Connection security mode. Values:
sl_bt_connection_mode1_level1 (0x0): No security
sl_bt_connection_mode1_level2 (0x1): Unauthenticated pairing with encryption
sl_bt_connection_mode1_level3 (0x2): Authenticated pairing with encryption
sl_bt_connection_mode1_level4 (0x3): Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key
5604
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
txsize#
uint16_t sl_bt_evt_connection_parameters_s::txsize
Deprecated and no longer used for reporting the connection data length update. Use the event sl_bt_evt_connection_data_length instead.
5616
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h