sl_bt_evt_cs_read_remote_supported_capabilities_complete#
Report the remote controller's supported capabilities as a result of calling the sl_bt_cs_read_remote_supported_capabilities command previously.
Modules#
sl_bt_evt_cs_read_remote_supported_capabilities_complete_s
Typedefs#
Macros#
#define
Identifier of the read_remote_supported_capabilities_complete event.
Typedef Documentation#
sl_bt_evt_cs_read_remote_supported_capabilities_complete_t#
typedef struct sl_bt_evt_cs_read_remote_supported_capabilities_complete_s sl_bt_evt_cs_read_remote_supported_capabilities_complete_t
Definition at line
12308
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_cs_read_remote_supported_capabilities_complete_id#
#define sl_bt_evt_cs_read_remote_supported_capabilities_complete_idValue:
0x045900a0
Identifier of the read_remote_supported_capabilities_complete event.
Definition at line
12092
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h