sl_bt_evt_cs_security_enable_complete#
Indicates that a locally initiated CS security start procedure has completed or the local controller has responded to a channel security request from the remote controller.
Modules#
sl_bt_evt_cs_security_enable_complete_s
Typedefs#
Macros#
#define
sl_bt_evt_cs_security_enable_complete_id 0x005900a0
Identifier of the security_enable_complete event.
Typedef Documentation#
sl_bt_evt_cs_security_enable_complete_t#
typedef struct sl_bt_evt_cs_security_enable_complete_s sl_bt_evt_cs_security_enable_complete_t
Definition at line
11627
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_cs_security_enable_complete_id#
#define sl_bt_evt_cs_security_enable_complete_idValue:
0x005900a0
Identifier of the security_enable_complete event.
Definition at line
11617
of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h