Bluetooth Mesh Diagnostic Utilities#
Bluetooth Mesh Diagnostic Utilities.
Diagnostic Utilities. It provides the functionality that assist with diagnosing problems.
Modules#
sl_btmesh_evt_diagnostic_relay
sl_btmesh_evt_diagnostic_friend_queue
sl_btmesh_evt_diagnostic_friend_relay
sl_btmesh_evt_diagnostic_friend_remove
Functions#
Macros#
Function Documentation#
sl_btmesh_diagnostic_init#
sl_status_t sl_btmesh_diagnostic_init ()
Initialize Diagnostic Utilities.
Returns
SL_STATUS_OK if successful. Error code otherwise.
22473
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_diagnostic_deinit#
sl_status_t sl_btmesh_diagnostic_deinit ()
Deinitialize Diagnostic Utilities. After this call it cannot be used until it is initialized again. See sl_btmesh_diagnostic_init.
Returns
SL_STATUS_OK if successful. Error code otherwise.
22484
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_diagnostic_enable_relay#
sl_status_t sl_btmesh_diagnostic_enable_relay ()
Enable event sending for each relayed or proxied message. NOTE: On NCP target this can saturate the NCP PHY interface. An alternative for this is sl_btmesh_diagnostic_get_relay
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
22499
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_diagnostic_disable_relay#
sl_status_t sl_btmesh_diagnostic_disable_relay ()
Disable event sending for each relayed or proxied message.
Returns
SL_STATUS_OK if successful. Error code otherwise.
22509
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_diagnostic_get_relay#
sl_status_t sl_btmesh_diagnostic_get_relay (uint32_t * relay_counter)
[out] | relay_counter | Relayed or proxied message counter. |
Get relayed or proxied message counter, which is a counter incremented for each relayed or proxied message.
Returns
SL_STATUS_OK if successful. Error code otherwise.
22521
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_diagnostic_get_statistics#
sl_status_t sl_btmesh_diagnostic_get_statistics (uint32_t requested_chunk, uint32_t requested_offset, uint32_t * total_length, uint32_t * chunk_offset, size_t max_statistics_size, size_t * statistics_len, uint8_t * statistics)
[in] | requested_chunk | Size of the statistics data chunk requested |
[in] | requested_offset | Byte offset to the statistics data chunk requested |
[out] | total_length | Total length of the statistics data in the system |
[out] | chunk_offset | Byte offset to the statistics data chunk delivered |
[in] | max_statistics_size | Size of output buffer passed in |
[out] | statistics_len | On return, set to the length of output data written to |
[out] | statistics | Raw statistics data counter array. |
Get a chunk of Bluetooth mesh stack statistics data counters. As there can be a large amount of statistics, it has to be retrieved as chunks. The application is free to specify the size of the chunk it wants to use, but keep in mind that for the NCP use case there may be limited size buffers in the underlying serial channel.
Returns
SL_STATUS_OK if successful. Error code otherwise.
22544
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_diagnostic_clear_statistics#
sl_status_t sl_btmesh_diagnostic_clear_statistics ()
Clear Bluetooth mesh stack statistics data counters.
Returns
SL_STATUS_OK if successful. Error code otherwise.
22560
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_diagnostic_enable_friend#
sl_status_t sl_btmesh_diagnostic_enable_friend ()
Enable event sending for friendship diagnostics on the friend node side. NOTE: On NCP target this can saturate the NCP PHY interface. An alternative for this is sl_btmesh_diagnostic_get_friend
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
22577
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_diagnostic_disable_friend#
sl_status_t sl_btmesh_diagnostic_disable_friend ()
Disable event sending for friendship diagnostics on the friend node side.
Returns
SL_STATUS_OK if successful. Error code otherwise.
22587
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_diagnostic_get_friend#
sl_status_t sl_btmesh_diagnostic_get_friend (uint32_t * queue_counter, uint32_t * relay_counter, uint32_t * remove_counter_sent, uint32_t * remove_counter_old_pdu, uint32_t * remove_counter_old_segack, uint32_t * remove_counter_old_segment)
[out] | queue_counter | Number of messages queued for LPNs. |
[out] | relay_counter | Number of messages relayed to LPNs as a response to polls. |
[out] | remove_counter_sent | Number of messages discarded from LPN friendship queues due to message having been to sent to LPN and acknowledged by LPN by it sending the next poll. |
[out] | remove_counter_old_pdu | Number of messages discarded from LPN friendship queues due to message queue overflow, resulting in the need to flush the oldest PDU un the queue |
[out] | remove_counter_old_segack | Number of messages discarded from LPN friendship queues due to a new segment acknowledgement message replacing an old one in the queue. |
[out] | remove_counter_old_segment | Number of messages discarded from LPN friendship queues due to invalidated segments being removed from the queue. |
Get friend event counters.
Returns
SL_STATUS_OK if successful. Error code otherwise.
22611
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_cmd_diagnostic_init_id#
#define sl_btmesh_cmd_diagnostic_init_idValue:
0x006c0028
22329
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_cmd_diagnostic_deinit_id#
#define sl_btmesh_cmd_diagnostic_deinit_idValue:
0x016c0028
22330
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_cmd_diagnostic_enable_relay_id#
#define sl_btmesh_cmd_diagnostic_enable_relay_idValue:
0x026c0028
22331
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_cmd_diagnostic_disable_relay_id#
#define sl_btmesh_cmd_diagnostic_disable_relay_idValue:
0x036c0028
22332
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_cmd_diagnostic_get_relay_id#
#define sl_btmesh_cmd_diagnostic_get_relay_idValue:
0x046c0028
22333
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_cmd_diagnostic_get_statistics_id#
#define sl_btmesh_cmd_diagnostic_get_statistics_idValue:
0x056c0028
22334
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_cmd_diagnostic_clear_statistics_id#
#define sl_btmesh_cmd_diagnostic_clear_statistics_idValue:
0x066c0028
22335
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_cmd_diagnostic_enable_friend_id#
#define sl_btmesh_cmd_diagnostic_enable_friend_idValue:
0x076c0028
22336
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_cmd_diagnostic_disable_friend_id#
#define sl_btmesh_cmd_diagnostic_disable_friend_idValue:
0x086c0028
22337
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_cmd_diagnostic_get_friend_id#
#define sl_btmesh_cmd_diagnostic_get_friend_idValue:
0x096c0028
22338
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_rsp_diagnostic_init_id#
#define sl_btmesh_rsp_diagnostic_init_idValue:
0x006c0028
22339
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_rsp_diagnostic_deinit_id#
#define sl_btmesh_rsp_diagnostic_deinit_idValue:
0x016c0028
22340
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_rsp_diagnostic_enable_relay_id#
#define sl_btmesh_rsp_diagnostic_enable_relay_idValue:
0x026c0028
22341
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_rsp_diagnostic_disable_relay_id#
#define sl_btmesh_rsp_diagnostic_disable_relay_idValue:
0x036c0028
22342
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_rsp_diagnostic_get_relay_id#
#define sl_btmesh_rsp_diagnostic_get_relay_idValue:
0x046c0028
22343
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_rsp_diagnostic_get_statistics_id#
#define sl_btmesh_rsp_diagnostic_get_statistics_idValue:
0x056c0028
22344
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_rsp_diagnostic_clear_statistics_id#
#define sl_btmesh_rsp_diagnostic_clear_statistics_idValue:
0x066c0028
22345
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_rsp_diagnostic_enable_friend_id#
#define sl_btmesh_rsp_diagnostic_enable_friend_idValue:
0x076c0028
22346
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_rsp_diagnostic_disable_friend_id#
#define sl_btmesh_rsp_diagnostic_disable_friend_idValue:
0x086c0028
22347
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_rsp_diagnostic_get_friend_id#
#define sl_btmesh_rsp_diagnostic_get_friend_idValue:
0x096c0028
22348
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h