Bluetooth Mesh Firmware Update Server Model#
Bluetooth Mesh Firmware Update Server Model.
This class provides the commands and messages to interface with the Firmware Update Server model.
The MBT Server must be initialized before the Update Server.
Modules#
sl_btmesh_evt_fw_update_server_check_fw_metadata_req
sl_btmesh_evt_fw_update_server_update_start_req
sl_btmesh_evt_fw_update_server_verify_fw_req
sl_btmesh_evt_fw_update_server_apply
sl_btmesh_evt_fw_update_server_update_cancelled
sl_btmesh_evt_fw_update_server_distributor_self_update_req
Enumerations#
The Update Phase of the Firmware Update Server.
Status codes reported by the Firmware Update Server.
Used by the implementation to accept or reject the image and select the status code reported by the Firmware Update Server.
Functions#
Macros#
Enumeration Documentation#
sl_btmesh_fw_update_server_update_phase_t#
sl_btmesh_fw_update_server_update_phase_t
The Update Phase of the Firmware Update Server.
Enumerator | |
---|---|
sl_btmesh_fw_update_server_update_phase_idle | (0x0) No firmware transfer is in progress. |
sl_btmesh_fw_update_server_update_phase_transfer_error | (0x1) Error occurred during firmware image BLOB transfer. |
sl_btmesh_fw_update_server_update_phase_transfer_in_progress | (0x2) Firmware image BLOB transfer is in progress. |
sl_btmesh_fw_update_server_update_phase_verifying_update | (0x3) Firmware image transfer completed, and the node is verifying the image. |
sl_btmesh_fw_update_server_update_phase_verification_success | (0x4) Firmware image verification succeeded. |
sl_btmesh_fw_update_server_update_phase_verification_failed | (0x5) Firmware image verification failed. |
sl_btmesh_fw_update_server_update_phase_apply_in_progress | (0x6) The node is applying the firmware image. |
15558
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_update_server_update_status_t#
sl_btmesh_fw_update_server_update_status_t
Status codes reported by the Firmware Update Server.
Enumerator | |
---|---|
sl_btmesh_fw_update_server_update_status_success | (0x0) The message was processed successfully. |
sl_btmesh_fw_update_server_update_status_out_of_resources | (0x1) Insufficient resources on the node. |
sl_btmesh_fw_update_server_update_status_wrong_phase | (0x2) The operation cannot be performed while the server is in the current phase. |
sl_btmesh_fw_update_server_update_status_internal_error | (0x3) An internal error occurred on the node. |
sl_btmesh_fw_update_server_update_status_wrong_fw_index | (0x4) The message contained a firmware index value that is not expected. |
sl_btmesh_fw_update_server_update_status_metadata_check_failed | (0x5) The firmware metadata check failed. |
sl_btmesh_fw_update_server_update_status_temporarily_unable | (0x6) The server cannot start a firmware update right now. |
sl_btmesh_fw_update_server_update_status_blob_transfer_busy | (0x7) The local MBT Server model is busy with another BLOB transfer. |
15623
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_update_server_update_start_response_type_t#
sl_btmesh_fw_update_server_update_start_response_type_t
Used by the implementation to accept or reject the image and select the status code reported by the Firmware Update Server.
Enumerator | |
---|---|
sl_btmesh_fw_update_server_update_start_response_type_accept | (0x0) Accept; the MBT Server will start receiving the image. |
sl_btmesh_fw_update_server_update_start_response_type_fw_already_exists | (0x1) Accept; the MBT Server will not start receiving the image, as the image has already been received. |
sl_btmesh_fw_update_server_update_start_response_type_reject_out_of_resources | (0x2) Reject; insufficient resources on the node. |
sl_btmesh_fw_update_server_update_start_response_type_reject_internal_error | (0x3) Reject; An internal error occurred on the node. |
sl_btmesh_fw_update_server_update_start_response_type_reject_metadata_check_failed | (0x4) Reject; the firmware metadata indicated that the image is not suitable for this node. |
sl_btmesh_fw_update_server_update_start_response_type_reject_temporarily_unable | (0x5) Reject; The server cannot start a firmware update right now. |
15713
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Function Documentation#
sl_btmesh_fw_update_server_init#
sl_status_t sl_btmesh_fw_update_server_init (uint16_t elem_index, uint8_t num_installed_fw, uint8_t max_metadata_len)
[in] | elem_index | Server model element index |
[in] | num_installed_fw | Number of installed FWs |
[in] | max_metadata_len | Maximum length of metadata supported. Any request with a larger metadata value will be rejected automatically. |
Initializes the Firmware Update Server model.
Returns
SL_STATUS_OK if successful. Error code otherwise.
15973
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_update_server_deinit#
sl_status_t sl_btmesh_fw_update_server_deinit (uint16_t elem_index)
[in] | elem_index | Server model element index |
Deinitializes the Firmware Update Server model.
Returns
SL_STATUS_OK if successful. Error code otherwise.
15986
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_update_server_check_fw_metadata_rsp#
sl_status_t sl_btmesh_fw_update_server_check_fw_metadata_rsp (uint16_t elem_index, uint8_t response_type, uint8_t additional_information, uint8_t fw_index)
[in] | elem_index | Server model element index |
[in] | response_type | Enum sl_btmesh_fw_update_server_update_start_response_type_t. The status code to indicate to the client. |
[in] | additional_information | Enum sl_btmesh_fw_update_client_additional_info_t. Additional information about what will happen to the node after the update is applied. 0 = no changes to DCD; 1 = DCD will change but Composition Data Refresh is not supported; 2 = DCD change and Composition Data Refresh is supported; 3 = node will become unprovisioned. |
[in] | fw_index | Index of the firmware to be updated. |
Response for the sl_btmesh_evt_fw_update_server_check_fw_metadata_req event. Report whether a server can accept a firmware update.
Returns
SL_STATUS_OK if successful. Error code otherwise.
16008
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_update_server_update_start_rsp#
sl_status_t sl_btmesh_fw_update_server_update_start_rsp (uint16_t elem_index, uint8_t response_type, uint8_t additional_information)
[in] | elem_index | Server model element index |
[in] | response_type | Enum sl_btmesh_fw_update_server_update_start_response_type_t. Accept or reject the image. |
[in] | additional_information | Enum sl_btmesh_fw_update_client_additional_info_t. Additional information about what will happen to the node after the update is applied. 0 = no changes to DCD; 1 = DCD will change but Composition Data Refresh is not supported; 2 = DCD change and Composition Data Refresh is supported; 3 = node will become unprovisioned. |
Response for the sl_btmesh_evt_fw_update_server_update_start_req event. After the firmware BLOB Transfer reception is complete, the event sl_btmesh_evt_fw_update_server_verify_fw_req will be generated.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
16036
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_update_server_verify_fw_rsp#
sl_status_t sl_btmesh_fw_update_server_verify_fw_rsp (uint16_t elem_index, uint8_t accept)
[in] | elem_index | Server model element index |
[in] | accept | 0 to reject the firmware image, nonzero to accept. If rejected, the server will indicate verification failure to the client when queried. If accepted, the server will wait for an apply command from the client. |
Response for the sl_btmesh_evt_fw_update_server_verify_fw_req event. If the image was accepted, the event sl_btmesh_evt_fw_update_server_apply will be generated when the Update Client asks the node to apply the new firmware and reboot.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
16059
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_update_server_distributor_self_update_rsp#
sl_status_t sl_btmesh_fw_update_server_distributor_self_update_rsp (uint16_t elem_index, uint8_t response_type, uint8_t additional_information)
[in] | elem_index | Server model element index |
[in] | response_type | Enum sl_btmesh_fw_update_server_update_start_response_type_t. Accept or reject the image. |
[in] | additional_information | Enum sl_btmesh_fw_update_client_additional_info_t. Additional information about what will happen to the node after the update is applied. 0 = no changes to DCD; 1 = DCD will change but Composition Data Refresh is not supported; 2 = DCD change and Composition Data Refresh is supported; 3 = node will become unprovisioned. |
Response for the sl_btmesh_evt_fw_update_server_distributor_self_update_req event. This command can only be used if both Distribution Server and Update Server functionality are used on the same node. If the self-update is accepted, the event sl_btmesh_evt_fw_update_server_verify_fw_req will be generated to confirm that the firmware image passed the application-specific checks, just like in a regular update.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
16089
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h