Bluetooth Mesh Remote Provisioning Server Model#

Bluetooth Mesh Remote Provisioning Server Model.

Remote Provisioning Server model provides tunneling of the provisioning commands for the provisioning process.

Modules#

sl_btmesh_evt_remote_provisioning_server_link_open_request

sl_btmesh_evt_remote_provisioning_server_link_close_request

Enumerations#

enum
sl_btmesh_remote_provisioning_server_idle = 0x0
sl_btmesh_remote_provisioning_server_multiple = 0x1
sl_btmesh_remote_provisioning_server_single = 0x2
}

Remote provisionin scan states.

enum
sl_btmesh_remote_provisioning_server_success = 0x0
sl_btmesh_remote_provisioning_server_scan_cannot_Start = 0x1
sl_btmesh_remote_provisioning_server_invalid_state = 0x2
sl_btmesh_remote_provisioning_server_limited_resources = 0x3
sl_btmesh_remote_provisioning_server_link_cannot_open = 0x4
sl_btmesh_remote_provisioning_server_link_open_failed = 0x5
sl_btmesh_remote_provisioning_server_link_closed_by_device = 0x6
sl_btmesh_remote_provisioning_server_link_closed_by_server = 0x7
sl_btmesh_remote_provisioning_server_link_closed_by_client = 0x8
sl_btmesh_remote_provisioning_server_link_closed_as_cannot_receive_pdu = 0x9
sl_btmesh_remote_provisioning_server_link_closed_as_cannot_send_pdu = 0xa
sl_btmesh_remote_provisioning_server_link_closed_as_cannot_deliver_pdu_report = 0xb
}

Remote provisionnin server status.

Enumeration Documentation#

sl_btmesh_remote_provisioning_server_scan_state_t#

sl_btmesh_remote_provisioning_server_scan_state_t

Remote provisionin scan states.

Enumerator
sl_btmesh_remote_provisioning_server_idle

(0x0) Idle state

sl_btmesh_remote_provisioning_server_multiple

(0x1) Multiple Devices Scan

sl_btmesh_remote_provisioning_server_single

(0x2) Single Device Scan


Definition at line 19548 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_remote_provisioning_server_status_t#

sl_btmesh_remote_provisioning_server_status_t

Remote provisionnin server status.

Enumerator
sl_btmesh_remote_provisioning_server_success

(0x0) Success

sl_btmesh_remote_provisioning_server_scan_cannot_Start

(0x1) Scanning Cannot Start

sl_btmesh_remote_provisioning_server_invalid_state

(0x2) Invalid State

sl_btmesh_remote_provisioning_server_limited_resources

(0x3) Limited Resources

sl_btmesh_remote_provisioning_server_link_cannot_open

(0x4) Link Cannot Open

sl_btmesh_remote_provisioning_server_link_open_failed

(0x5) Link open failed

sl_btmesh_remote_provisioning_server_link_closed_by_device

(0x6) Link Closed by Device

sl_btmesh_remote_provisioning_server_link_closed_by_server

(0x7) Link closed by server

sl_btmesh_remote_provisioning_server_link_closed_by_client

(0x8) Link closed by client

sl_btmesh_remote_provisioning_server_link_closed_as_cannot_receive_pdu

(0x9) Link closed as cannot receive PDU

sl_btmesh_remote_provisioning_server_link_closed_as_cannot_send_pdu

(0xa) Link closed as cannot send PDU

sl_btmesh_remote_provisioning_server_link_closed_as_cannot_deliver_pdu_report

(0xb) Link closed as cannot deliver PDU report


Definition at line 19560 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Function Documentation#

sl_btmesh_remote_provisioning_server_init#

sl_status_t sl_btmesh_remote_provisioning_server_init ()

Initialize the remote provisioning server.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 19691 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_remote_provisioning_server_open_link#

sl_status_t sl_btmesh_remote_provisioning_server_open_link (uint8_t connection)
Parameters
[in]connection

Handle that was assigned to the connection

This command is used to pass connction handle to the remote provisioning server after having received sl_btmesh_evt_remote_provisioning_server_link_open_request event.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 19707 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_remote_provisioning_server_set_default_bearer#

sl_status_t sl_btmesh_remote_provisioning_server_set_default_bearer (uint8_t bearer)
Parameters
[in]bearer

Default bearer for provisioning.

  • 1 PB-ADV

  • 2 PB-GATT

Set default bearer to be used in remote provisioning.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 19723 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_cmd_remote_provisioning_server_init_id#

#define sl_btmesh_cmd_remote_provisioning_server_init_id
Value:
0x00310028

Definition at line 19538 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_remote_provisioning_server_open_link_id#

#define sl_btmesh_cmd_remote_provisioning_server_open_link_id
Value:
0x01310028

Definition at line 19539 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_cmd_remote_provisioning_server_set_default_bearer_id#

#define sl_btmesh_cmd_remote_provisioning_server_set_default_bearer_id
Value:
0x02310028

Definition at line 19540 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_remote_provisioning_server_init_id#

#define sl_btmesh_rsp_remote_provisioning_server_init_id
Value:
0x00310028

Definition at line 19541 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_remote_provisioning_server_open_link_id#

#define sl_btmesh_rsp_remote_provisioning_server_open_link_id
Value:
0x01310028

Definition at line 19542 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sl_btmesh_rsp_remote_provisioning_server_set_default_bearer_id#

#define sl_btmesh_rsp_remote_provisioning_server_set_default_bearer_id
Value:
0x02310028

Definition at line 19543 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h