Bluetooth Mesh Firmware Distribution Server Model#
Bluetooth Mesh Firmware Distribution Server Model.
The Bluetooth Mesh Firmware Distribution Server Model is used to receive new firmware images from the Firmware Distribution Client model and distribute them to Target Nodes. As a transport layer Bluetooth Mesh BLOB Transfer (MBT) models are in use.
Modules#
sl_btmesh_evt_fw_dist_server_nodes_added
sl_btmesh_evt_fw_dist_server_nodes_deleted
sl_btmesh_evt_fw_dist_server_dist_start_req
sl_btmesh_evt_fw_dist_server_dist_cancel
sl_btmesh_evt_fw_dist_server_dist_cancel_complete
sl_btmesh_evt_fw_dist_server_upload_start_metadata
sl_btmesh_evt_fw_dist_server_upload_start_req
sl_btmesh_evt_fw_dist_server_upload_cancel
sl_btmesh_evt_fw_dist_server_dist_state_changed
sl_btmesh_evt_fw_dist_server_node_failed
sl_btmesh_evt_fw_dist_server_upload_complete_metadata
sl_btmesh_evt_fw_dist_server_upload_complete
sl_btmesh_evt_fw_dist_server_upload_failed
sl_btmesh_evt_fw_dist_server_upload_oob_start_uri
sl_btmesh_evt_fw_dist_server_upload_oob_start_req
sl_btmesh_evt_fw_dist_server_fw_delete_req
sl_btmesh_evt_fw_dist_server_fw_delete_all_req
sl_btmesh_evt_fw_dist_server_dist_suspend
sl_btmesh_evt_fw_dist_server_resume_req
Enumerations#
The state machine states of the Distribution Server's distribution procedure.
The Update Policy determines whether the Distribution Server will send Update Apply messages to the Target Nodes immediately, or wait for the Distribution Client to send it the Distribution Apply message.
The phase of the Target Node as determined by the Distribution Server.
Status codes reported by the Firmware Distribution Server.
Functions#
Macros#
Enumeration Documentation#
sl_btmesh_fw_dist_server_dist_step_t#
sl_btmesh_fw_dist_server_dist_step_t
The state machine states of the Distribution Server's distribution procedure.
Enumerator | |
---|---|
sl_btmesh_fw_dist_server_dist_step_idle | (0x0) No distribution is active. |
sl_btmesh_fw_dist_server_dist_step_starting_update | (0x1) Sending Update Start messages. |
sl_btmesh_fw_dist_server_dist_step_transferring_image | (0x2) Firmware image BLOB transfer is in progress. |
sl_btmesh_fw_dist_server_dist_step_checking_verification | (0x3) Sending Update Get messages to check verification status. |
sl_btmesh_fw_dist_server_dist_step_waiting_for_apply | (0x4) Park state if Update Policy is Verify Only: wait for Distribution Apply. If the policy is Verify and Apply, this state is skipped. |
sl_btmesh_fw_dist_server_dist_step_applying_update | (0x5) Sending Update Apply messages. |
sl_btmesh_fw_dist_server_dist_step_checking_update_result | (0x6) Sending Information Get messages to determine if new firmware was applied. |
sl_btmesh_fw_dist_server_dist_step_completed | (0x7) Completed successfully for at least one Target Node. |
sl_btmesh_fw_dist_server_dist_step_failed | (0x8) Distribution failed for all Target Nodes. |
sl_btmesh_fw_dist_server_dist_step_cancelling | (0x9) Cancelling an ongoing distribution. |
sl_btmesh_fw_dist_server_dist_step_suspended | (0xa) Firmware image BLOB transfer is temporarily suspended. |
16930
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_dfu_policy_t#
sl_btmesh_fw_dist_server_dfu_policy_t
The Update Policy determines whether the Distribution Server will send Update Apply messages to the Target Nodes immediately, or wait for the Distribution Client to send it the Distribution Apply message.
Enumerator | |
---|---|
sl_btmesh_fw_dist_server_dfu_policy_verify_only | (0x0) The Distribution Server will wait for the Distribution Apply message, and then send the Update Apply messages. |
sl_btmesh_fw_dist_server_dfu_policy_verify_and_apply | (0x1) The Distribution Server will send the Update Apply messages immediately, after the firmware image verification is complete. |
17026
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_dist_node_phase_t#
sl_btmesh_fw_dist_server_dist_node_phase_t
The phase of the Target Node as determined by the Distribution Server.
Enumerator | |
---|---|
sl_btmesh_fw_dist_server_dist_node_phase_idle | (0x0) No firmware transfer is in progress. |
sl_btmesh_fw_dist_server_dist_node_phase_transfer_error | (0x1) Error occurred during firmware image BLOB transfer. |
sl_btmesh_fw_dist_server_dist_node_phase_transfer_in_progress | (0x2) Firmware image BLOB transfer is in progress. |
sl_btmesh_fw_dist_server_dist_node_phase_verifying_update | (0x3) Firmware image transfer completed, and the node is verifying the image. |
sl_btmesh_fw_dist_server_dist_node_phase_verification_success | (0x4) Firmware image verification succeeded. |
sl_btmesh_fw_dist_server_dist_node_phase_verification_failed | (0x5) Firmware image verification failed. |
sl_btmesh_fw_dist_server_dist_node_phase_apply_in_progress | (0x6) The node is applying the firmware update. |
sl_btmesh_fw_dist_server_dist_node_phase_transfer_cancelled | (0x7) Firmware transfer was cancelled. |
sl_btmesh_fw_dist_server_dist_node_phase_apply_success | (0x8) Firmware was applied successfully. |
sl_btmesh_fw_dist_server_dist_node_phase_apply_failed | (0x9) Firmware applying failed. |
sl_btmesh_fw_dist_server_dist_node_phase_unknown | (0xa) The phase of the node has not been retrieved yet. |
17055
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_dist_status_t#
sl_btmesh_fw_dist_server_dist_status_t
Status codes reported by the Firmware Distribution Server.
Enumerator | |
---|---|
sl_btmesh_fw_dist_server_dist_status_success | (0x0) The message was processed successfully. |
sl_btmesh_fw_dist_server_dist_status_out_of_resources | (0x1) Insufficient resources on the node. |
sl_btmesh_fw_dist_server_dist_status_wrong_phase | (0x2) The operation cannot be performed while the server is in the current phase. |
sl_btmesh_fw_dist_server_dist_status_internal_error | (0x3) An internal error occurred on the node. |
sl_btmesh_fw_dist_server_dist_status_fwid_not_found | (0x4) The requested firmware image is not stored on the server. |
sl_btmesh_fw_dist_server_dist_status_invalid_appkey_index | (0x5) The appkey identified by the appkey index is not known. |
sl_btmesh_fw_dist_server_dist_status_receivers_list_empty | (0x6) There are no Target Nodes in the Distribution Receivers List. |
sl_btmesh_fw_dist_server_dist_status_busy_with_distribution | (0x7) Another distribution is already in progress. |
sl_btmesh_fw_dist_server_dist_status_busy_with_upload | (0x8) Another upload is already in progress. |
sl_btmesh_fw_dist_server_dist_status_uri_not_supported | (0x9) The URI scheme name indicated by the URI is not supported. |
sl_btmesh_fw_dist_server_dist_status_uri_malformed | (0xa) The format of the URI is invalid. |
sl_btmesh_fw_dist_server_dist_status_uri_unreachable | (0xb) The URI is currently unreachable. |
sl_btmesh_fw_dist_server_dist_status_new_fw_not_available | (0xc) No new firmware was available with given the URI + Current FWID. |
sl_btmesh_fw_dist_server_dist_status_suspend_failed | (0xd) Suspending a distribution failed. |
17151
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Function Documentation#
sl_btmesh_fw_dist_server_init#
sl_status_t sl_btmesh_fw_dist_server_init (uint16_t elem_index, uint16_t max_node_list_size, uint16_t max_fw_entries, uint32_t max_fw_size, uint32_t total_store_size, uint16_t multicast_threshold, size_t oob_supported_uri_scheme_names_len, const uint8_t * oob_supported_uri_scheme_names)
[in] | elem_index | Server model element index |
[in] | max_node_list_size | Maximum number of nodes that can be updated simultaneously |
[in] | max_fw_entries | Maximum number of firmware images that can be stored |
[in] | max_fw_size | Maximum size of a single firmware image |
[in] | total_store_size | Maximum combined size of all firmware images |
[in] | multicast_threshold | This value will be passed to the MBT Client. If the number of servers for any step exceeds or is equal to this number, the group address will be used. Otherwise, servers will be looped through one by one. Value of 0 disables the feature. |
[in] | oob_supported_uri_scheme_names_len | Length of data in |
[in] | oob_supported_uri_scheme_names | To indicate Upload OOB support, list the supported URI Scheme Names UTF-8 code points here (see https://www.bluetooth.com/specifications/assigned-numbers/uri-scheme-name-string-mapping/). To indicate Upload OOB is not supported, give a zero-length string. |
Initializes the Firmware Distribution Server model. Before initializing the Distribution Server model, the Update Client and MBT Server models on the same element must be initialized.
Returns
SL_STATUS_OK if successful. Error code otherwise.
17777
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_deinit#
sl_status_t sl_btmesh_fw_dist_server_deinit (uint16_t elem_index)
[in] | elem_index | Server model element index |
Deinitializes the Firmware Distribution Server model. The corresponding Update Client and MBT Server models can be deinitialized before or after this model.
Returns
SL_STATUS_OK if successful. Error code otherwise.
17797
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_upload_start_rsp#
sl_status_t sl_btmesh_fw_dist_server_upload_start_rsp (uint16_t elem_index, uint8_t status)
[in] | elem_index | Server model element index |
[in] | status | Enum sl_btmesh_fw_dist_server_dist_status_t. Status code to the client |
Response for the upload_start_req event
Returns
SL_STATUS_OK if successful. Error code otherwise.
17810
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_execute_distribution_step#
sl_status_t sl_btmesh_fw_dist_server_execute_distribution_step (uint16_t elem_index)
[in] | elem_index | Server model element index |
Execute the next action for the distribution state machine.
Returns
SL_STATUS_OK if successful. Error code otherwise.
17822
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_upload_oob_start_rsp#
sl_status_t sl_btmesh_fw_dist_server_upload_oob_start_rsp (uint16_t elem_index, uint8_t status_code, size_t fwid_len, const uint8_t * fwid)
[in] | elem_index | Server model element index |
[in] | status_code | Enum sl_btmesh_fw_dist_server_dist_status_t. Status code to use for the response. Must be one of the following:
All other status codes are reserved or automatically sent by the stack. |
[in] | fwid_len | Length of data in |
[in] | fwid | Firmware ID of the image that will be retrieved OOB. The Firmware ID is retrieved by executing the Check Firmware OOB procedure. |
Response to the sl_btmesh_evt_fw_dist_server_upload_oob_start_req event. The application should run the Check Firmware OOB procedure (as detailed in the specification) in order to check that the given URI is reachable, and a new firmware image is available.
When the size of the image is known, sl_btmesh_fw_dist_server_set_upload_oob_image_size must be called to inform the stack about the size of the image.
If the image has an associated set of metadata, sl_btmesh_fw_dist_server_set_upload_oob_metadata must be called to inform the stack about the image metadata.
The command sl_btmesh_fw_dist_server_set_upload_oob_progress must be called at minimum when the transfer completes or an error is encountered. It can be called earlier to inform the stack about the transfer progress.
Returns
SL_STATUS_OK if successful. Error code otherwise.
17865
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_set_upload_oob_metadata#
sl_status_t sl_btmesh_fw_dist_server_set_upload_oob_metadata (uint16_t elem_index, size_t metadata_len, const uint8_t * metadata)
[in] | elem_index | Server model element index |
[in] | metadata_len | Length of data in |
[in] | metadata | Metadata of the image. May be zero-length. |
Set the metadata of an image retrieved via OOB Upload. This command can be used after sl_btmesh_fw_dist_server_upload_oob_start_rsp, and cannot be used after the OOB Upload completes. If the uploaded firmware image has no associated metadata, this command does not need to be called.
Returns
SL_STATUS_OK if successful. Error code otherwise.
17884
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_set_upload_oob_image_size#
sl_status_t sl_btmesh_fw_dist_server_set_upload_oob_image_size (uint16_t elem_index, uint32_t size)
[in] | elem_index | Server model element index |
[in] | size | Size of the new firmware image |
Set the size of the image being retrieved via OOB Upload. This command must be used after sl_btmesh_fw_dist_server_upload_oob_start_rsp, as soon as the size of the image is known. The upload cannot be completed with sl_btmesh_fw_dist_server_set_upload_oob_progress before the size is set.
Returns
SL_STATUS_OK if successful. Error code otherwise.
17901
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_set_upload_oob_progress#
sl_status_t sl_btmesh_fw_dist_server_set_upload_oob_progress (uint16_t elem_index, uint8_t error, uint8_t progress, uint16_t * fw_list_index)
[in] | elem_index | Server model element index |
[in] | error | Set to zero if no error occurred. If nonzero, the transfer will be considered a failure, and the Upload Phase will be set to Transfer Error. A nonzero value cannot be used in conjuction with progress 100. Note that there is no way in the specification to indicate what kind of error occurred during the OOB retrieval. Only the initial start request can be rejected with a specific error code; see sl_btmesh_fw_dist_server_upload_oob_start_rsp. |
[in] | progress | Progress of the transfer, in percentage. Range: 0-100. If set 100, the upload will be completed, and the fw_list_index return parameter is populated with the Firmware List Index that was assigned to the new image. |
[out] | fw_list_index | Firmware List Index that was assigned to the image, if progress was set to 100. Otherwise will be set to 0xffff, and should be ignored. |
Set the progress of the Upload OOB image retrieval. Used to inform the stack about the progress, and to indicate when the process is complete.
Returns
SL_STATUS_OK if successful. Error code otherwise.
17931
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_get_node_status_by_index#
sl_status_t sl_btmesh_fw_dist_server_get_node_status_by_index (uint16_t elem_index, uint16_t entry_index, uint16_t * address, uint8_t * retrieved_phase, uint8_t * update_server_status, uint8_t * mbt_server_status, uint8_t * transfer_progress, uint8_t * fw_index)
[in] | elem_index | Server model element index |
[in] | entry_index | Node entry index |
[out] | address | Address of the Update Server |
[out] | retrieved_phase | Enum sl_btmesh_fw_dist_server_dist_node_phase_t. Phase of the Update Server |
[out] | update_server_status | Enum sl_btmesh_fw_update_server_update_status_t. Last Update Status message received from the Update Server |
[out] | mbt_server_status | Enum sl_btmesh_mbt_server_status_t. Last Transfer Status message received from the BLOB Transfer Server |
[out] | transfer_progress | 0-100, percentage of BLOB Transfer octets delivered and confirmed |
[out] | fw_index | Index of the firmware being updated |
Retrieve information about the ongoing update on a node
Returns
SL_STATUS_OK if successful. Error code otherwise.
17957
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_get_node_status_by_address#
sl_status_t sl_btmesh_fw_dist_server_get_node_status_by_address (uint16_t elem_index, uint16_t node_address, uint16_t * address, uint8_t * retrieved_phase, uint8_t * update_server_status, uint8_t * mbt_server_status, uint8_t * transfer_progress, uint8_t * fw_index)
[in] | elem_index | Server model element index |
[in] | node_address | Node mesh address |
[out] | address | Address of the Update Server |
[out] | retrieved_phase | Enum sl_btmesh_fw_dist_server_dist_node_phase_t. Phase of the Update Server |
[out] | update_server_status | Enum sl_btmesh_fw_update_server_update_status_t. Last Update Status message received from the Update Server |
[out] | mbt_server_status | Enum sl_btmesh_mbt_server_status_t. Last Transfer Status message received from the BLOB Transfer Server |
[out] | transfer_progress | 0-100, percentage of BLOB Transfer octets delivered and confirmed |
[out] | fw_index | Index of the firmware being updated |
Retrieve information about the ongoing update by a node address
Returns
SL_STATUS_OK if successful. Error code otherwise.
17987
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_delete_rsp#
sl_status_t sl_btmesh_fw_dist_server_delete_rsp (uint16_t elem_index, uint16_t status, size_t fwid_len, const uint8_t * fwid)
[in] | elem_index | Server model element index |
[in] | status | Enum sl_btmesh_fw_dist_server_dist_status_t. Status code to use for the response. Must be one of the following:
All other status codes are reserved or automatically sent by the stack. |
[in] | fwid_len | Length of data in |
[in] | fwid | Firmware ID of the image that was requested to be deleted. |
Response to the sl_btmesh_evt_fw_dist_server_fw_delete_req event. The application should check that requested firmware image exists and can be deleted. The stack will ignore incoming sl_btmesh_fw_dist_client_start_distribution, sl_btmesh_fw_dist_client_start_upload, sl_btmesh_fw_dist_client_get_fw, sl_btmesh_fw_dist_client_get_fw_by_index, sl_btmesh_fw_dist_client_delete_all_fw commands until the response is called.
Returns
SL_STATUS_OK if successful. Error code otherwise.
18022
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_dist_start_rsp#
sl_status_t sl_btmesh_fw_dist_server_dist_start_rsp (uint16_t elem_index, uint16_t status)
[in] | elem_index | Server model element index |
[in] | status | mesh_dfu_dist_status_success to accept, mesh_dfu_dist_status_internal_error to reject |
Response to the sl_btmesh_evt_fw_dist_server_dist_start_req event. The stack will ignore incoming sl_btmesh_fw_dist_client_start_distribution, sl_btmesh_fw_dist_client_start_upload, sl_btmesh_fw_dist_client_get_fw, sl_btmesh_fw_dist_client_get_fw_by_index, sl_btmesh_fw_dist_client_delete_all_fw commands until the response is called.
Returns
SL_STATUS_OK if successful. Error code otherwise.
18043
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_set_multicast_threshold#
sl_status_t sl_btmesh_fw_dist_server_set_multicast_threshold (uint16_t elem_index, uint16_t multicast_threshold)
[in] | elem_index | Element index |
[in] | multicast_threshold | This value will be passed to the MBT Client. If the number of servers for any step exceeds or is equal to this number, the group address will be used. Otherwise, servers will be looped through one by one. Value of 0 disables the feature. |
Set the multicast threshold value.
Returns
SL_STATUS_OK if successful. Error code otherwise.
18059
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_delete_all_rsp#
sl_status_t sl_btmesh_fw_dist_server_delete_all_rsp (uint16_t elem_index, uint16_t status)
[in] | elem_index | Server model element index |
[in] | status | Enum sl_btmesh_fw_dist_server_dist_status_t. Status code to use for the response. Must be one of the following:
All other status codes are reserved or automatically sent by the stack. |
Response to the sl_btmesh_evt_fw_dist_server_fw_delete_all_req event. The application should check that all firmware images can be deleted. The stack will ignore incoming sl_btmesh_fw_dist_client_start_distribution, sl_btmesh_fw_dist_client_start_upload, sl_btmesh_fw_dist_client_get_fw, sl_btmesh_fw_dist_client_get_fw_by_index, sl_btmesh_fw_dist_client_delete_all_fw commands until the response is called.
Returns
SL_STATUS_OK if successful. Error code otherwise.
18086
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_fw_dist_server_resume_rsp#
sl_status_t sl_btmesh_fw_dist_server_resume_rsp (uint16_t elem_index, uint16_t status)
[in] | elem_index | Server model element index |
[in] | status | Enum sl_btmesh_fw_dist_server_dist_status_t. Status code to use for the response. Must be one of the following:
All other status codes are reserved or automatically sent by the stack. |
Response to the sl_btmesh_evt_fw_dist_server_resume_req event.
Returns
SL_STATUS_OK if successful. Error code otherwise.
18107
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h